<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC9S08JM32 SCI question</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM32-SCI-question/m-p/181325#M13176</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I will make some tests... more clearly now&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Receiving from the PC can be usefull to use the RxInterrupt in the MCU?&lt;/P&gt;&lt;P&gt;My program is very simple. PC says: "hey! send the data, and the MCU answers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Independtly of stop and wait mode, I think it´s more gently to "wake up" the MCU through the interrupt instead of seeking the buffer constantly in the main loop.&lt;/P&gt;&lt;P&gt;So I think this is the common way to receive data from the PC...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Feb 2011 17:53:24 GMT</pubDate>
    <dc:creator>Betadine</dc:creator>
    <dc:date>2011-02-04T17:53:24Z</dc:date>
    <item>
      <title>MC9S08JM32 SCI question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM32-SCI-question/m-p/181323#M13174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the first time I write the SCI code for RS232. The Processor Expert helps a lot, but I can´t understand a very simple question:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why I must activate interrupts for sending and receiving more than one character?&lt;/P&gt;&lt;P&gt;I only can edit the buffer size once I activate the IRQs... why it´s linked?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am I missing something?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Feb 2011 22:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM32-SCI-question/m-p/181323#M13174</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2011-02-03T22:41:34Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08JM32 SCI question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM32-SCI-question/m-p/181324#M13175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This must be a limitation imposed by Processor Expert as there is no necessity to do so imposed at the chip level. As long as you can poll in less than a byte time you don't need receive interrupts and unless there is some timing requirement imposed by the other end of your link you don't need transmit interrupts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Feb 2011 05:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM32-SCI-question/m-p/181324#M13175</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2011-02-04T05:00:04Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08JM32 SCI question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM32-SCI-question/m-p/181325#M13176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, I will make some tests... more clearly now&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Receiving from the PC can be usefull to use the RxInterrupt in the MCU?&lt;/P&gt;&lt;P&gt;My program is very simple. PC says: "hey! send the data, and the MCU answers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Independtly of stop and wait mode, I think it´s more gently to "wake up" the MCU through the interrupt instead of seeking the buffer constantly in the main loop.&lt;/P&gt;&lt;P&gt;So I think this is the common way to receive data from the PC...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Feb 2011 17:53:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08JM32-SCI-question/m-p/181325#M13176</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2011-02-04T17:53:24Z</dc:date>
    </item>
  </channel>
</rss>