<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: 9S08QG8 CWv10 eclipse printf issue</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179858#M12933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Search this forum for "TERMIO_PutChar", this came up in the past.&lt;/P&gt;&lt;P&gt;Basically you have to provide your own&amp;nbsp;TERMIO_PutChar/TERMIO_Init functions, there is a template in a file called termio,c when I remember correctly.&lt;/P&gt;&lt;P&gt;Note that this did not change in the MCU 10 release, while the user interface changed (now eclipse, previous a custom build environment), the libraries and the setup needed is still the same, so the old solutions should help you going.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 30 Jan 2011 13:28:52 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2011-01-30T13:28:52Z</dc:date>
    <item>
      <title>9S08QG8 CWv10 eclipse printf issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179857#M12932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having trouble getting printf to work on a simple 9S08QG8 program. &amp;nbsp;Using CW v10 on Windows Vista machine. &amp;nbsp;I loaded Ansiis.lib into the library. &amp;nbsp;It doesn't seem to be recognizing it. &amp;nbsp;Where is printf located in the new version of CW? &amp;nbsp;Here's my console build output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;**** Build of configuration MC9S08QG8 for project S08QG8demo ****&lt;/DIV&gt;&lt;DIV&gt;C:\Program Files (x86)\Freescale\CW MCU v10.0\gnu\bin\make all&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;'Building target: S08QG8demo.abs'&lt;/DIV&gt;&lt;DIV&gt;'Invoking: Linker'&lt;/DIV&gt;&lt;DIV&gt;"C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/prog/linker" -ArgFile"S08QG8demo.args" -O"S08QG8demo.abs" -Add("./Sources/Events.obj" "./Sources/ProcessorExpert.obj" "./Project_Settings/Startup_Code/start08.obj" "./Generated_Code/Bit1.obj" "./Generated_Code/Cpu.obj" "./Generated_Code/IO_Map.obj" "./Generated_Code/Vectors.obj" "C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib")&lt;/DIV&gt;&lt;DIV&gt;C:/Users/Sandman/workspace/S08QG8demo/Project_Settings/Linker_Files/ProcessorExpert.prm&lt;/DIV&gt;&lt;DIV&gt;Command Line: '-ArgFile"S08QG8demo.args" -O"S08QG8demo.abs" -Add("./Sources/Events.obj" "./Sources/ProcessorExpert.obj" "./Project_Settings/Startup_Code/start08.obj" "./Generated_Code/Bit1.obj" "./Generated_Code/Cpu.obj" "./Generated_Code/IO_Map.obj" "./Generated_Code/Vectors.obj" "C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib")'&lt;/DIV&gt;&lt;DIV&gt;Linking C:/Users/Sandman/workspace/S08QG8demo/Project_Settings/Linker_Files/ProcessorExpert.prm&lt;/DIV&gt;&lt;DIV&gt;Reading file './Sources/Events.obj'&lt;/DIV&gt;&lt;DIV&gt;Reading file './Sources/ProcessorExpert.obj'&lt;/DIV&gt;&lt;DIV&gt;Reading file './Project_Settings/Startup_Code/start08.obj'&lt;/DIV&gt;&lt;DIV&gt;Reading file './Generated_Code/Bit1.obj'&lt;/DIV&gt;&lt;DIV&gt;Reading file './Generated_Code/Cpu.obj'&lt;/DIV&gt;&lt;DIV&gt;Reading file './Generated_Code/IO_Map.obj'&lt;/DIV&gt;&lt;DIV&gt;Reading file './Generated_Code/Vectors.obj'&lt;/DIV&gt;&lt;DIV&gt;Reading file 'C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib'&lt;/DIV&gt;&lt;DIV&gt;ERROR L1822: Symbol TERMIO_PutChar in file C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib\ansiis.lib is undefined&lt;/DIV&gt;&lt;DIV&gt;Generating MAP file 'C:\Users\Sandman\workspace\S08QG8demo\MC9S08QG8\S08QG8demo.map'&lt;/DIV&gt;&lt;DIV&gt;SmartLinker: *** 1 error(s), 0 warning(s), 0 information message(s) ***&lt;/DIV&gt;&lt;DIV&gt;*** command line: '-ArgFile"S08QG8demo.args" -O"S08QG8demo.abs" -Add("./Sources/Events.obj" "./Sources/ProcessorExpert.obj" "./Project_Settings/Startup_Code/start08.obj" "./Generated_Code/Bit1.obj" "./Generated_Code/Cpu.obj" "./Generated_Code/IO_Map.obj" "./Generated_Code/Vectors.obj" "C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib")' ***&lt;/DIV&gt;&lt;DIV&gt;SmartLinker: *** Error occurred while processing! ***&lt;/DIV&gt;&lt;DIV&gt;C:\Program Files (x86)\Freescale\CW MCU v10.0\gnu\bin\make: *** [S08QG8demo.abs] Error 1&lt;/DIV&gt;&lt;P&gt;**** Build of configuration MC9S08QG8 for project S08QG8demo ****&lt;BR /&gt;C:\Program Files (x86)\Freescale\CW MCU v10.0\gnu\bin\make all&amp;nbsp;'Building target: S08QG8demo.abs''Invoking: Linker'"C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/prog/linker" -ArgFile"S08QG8demo.args" -O"S08QG8demo.abs" -Add("./Sources/Events.obj" "./Sources/ProcessorExpert.obj" "./Project_Settings/Startup_Code/start08.obj" "./Generated_Code/Bit1.obj" "./Generated_Code/Cpu.obj" "./Generated_Code/IO_Map.obj" "./Generated_Code/Vectors.obj" "C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib")C:/Users/Sandman/workspace/S08QG8demo/Project_Settings/Linker_Files/ProcessorExpert.prmCommand Line: '-ArgFile"S08QG8demo.args" -O"S08QG8demo.abs" -Add("./Sources/Events.obj" "./Sources/ProcessorExpert.obj" "./Project_Settings/Startup_Code/start08.obj" "./Generated_Code/Bit1.obj" "./Generated_Code/Cpu.obj" "./Generated_Code/IO_Map.obj" "./Generated_Code/Vectors.obj" "C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib")'Linking C:/Users/Sandman/workspace/S08QG8demo/Project_Settings/Linker_Files/ProcessorExpert.prmReading file './Sources/Events.obj'Reading file './Sources/ProcessorExpert.obj'Reading file './Project_Settings/Startup_Code/start08.obj'Reading file './Generated_Code/Bit1.obj'Reading file './Generated_Code/Cpu.obj'Reading file './Generated_Code/IO_Map.obj'Reading file './Generated_Code/Vectors.obj'Reading file 'C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib'ERROR L1822: Symbol TERMIO_PutChar in file C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib\ansiis.lib is undefinedGenerating MAP file 'C:\Users\Sandman\workspace\S08QG8demo\MC9S08QG8\S08QG8demo.map'SmartLinker: *** 1 error(s), 0 warning(s), 0 information message(s) ****** command line: '-ArgFile"S08QG8demo.args" -O"S08QG8demo.abs" -Add("./Sources/Events.obj" "./Sources/ProcessorExpert.obj" "./Project_Settings/Startup_Code/start08.obj" "./Generated_Code/Bit1.obj" "./Generated_Code/Cpu.obj" "./Generated_Code/IO_Map.obj" "./Generated_Code/Vectors.obj" "C:\Program Files (x86)\Freescale\CW MCU v10.0\eclipse\../MCU/lib/hc08c/lib/ansiis.lib")' ***SmartLinker: *** Error occurred while processing! ***C:\Program Files (x86)\Freescale\CW MCU v10.0\gnu\bin\make: *** [S08QG8demo.abs] Error 1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Jan 2011 13:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179857#M12932</guid>
      <dc:creator>Bubbaconch</dc:creator>
      <dc:date>2011-01-30T13:02:30Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08QG8 CWv10 eclipse printf issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179858#M12933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Search this forum for "TERMIO_PutChar", this came up in the past.&lt;/P&gt;&lt;P&gt;Basically you have to provide your own&amp;nbsp;TERMIO_PutChar/TERMIO_Init functions, there is a template in a file called termio,c when I remember correctly.&lt;/P&gt;&lt;P&gt;Note that this did not change in the MCU 10 release, while the user interface changed (now eclipse, previous a custom build environment), the libraries and the setup needed is still the same, so the old solutions should help you going.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Jan 2011 13:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179858#M12933</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2011-01-30T13:28:52Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08QG8 CWv10 eclipse printf issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179859#M12934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; you can reference this file.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.sparetimelabs.com/printfrevisited/tinyprinf-revised.zip" rel="nofollow" target="_self"&gt;Here&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Feb 2011 00:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179859#M12934</guid>
      <dc:creator>Mickey</dc:creator>
      <dc:date>2011-02-12T00:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08QG8 CWv10 eclipse printf issue</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179860#M12935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried the attached tiny format printf in the attachments but I still get compile error as "CompilerGuru" has said,&amp;nbsp; I get TERMIO_PutChar in file C:\.ProgramFiles\Freescale\CodeWarrior\lib\hc08c\lib\\ansif.lib is undefined&amp;nbsp; "Error" Linker Failed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Nov 2012 17:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08QG8-CWv10-eclipse-printf-issue/m-p/179860#M12935</guid>
      <dc:creator>jeff_sylvester</dc:creator>
      <dc:date>2012-11-02T17:52:42Z</dc:date>
    </item>
  </channel>
</rss>