<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ICG oscillator operation in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-oscillator-operation/m-p/179130#M12810</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bob,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After POR, the default operating mode for the ICG module will be FEI.&amp;nbsp; The crystal oscillator will be inoperative.&amp;nbsp; You will then&amp;nbsp;need to set ICGC1 to enable the oscillator, and to switch to FEE mode.&amp;nbsp; Refer to the datasheet, section 10.5.3, Example #2 for the required procedure.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Jul 2012 13:00:19 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2012-07-13T13:00:19Z</dc:date>
    <item>
      <title>ICG oscillator operation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-oscillator-operation/m-p/179129#M12809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Everybody;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;With a new (non programmed) 9S08AC60 and crystal (4 MHz), caps, resistor connected to xtal &amp;amp; extal pins. On the application of power, 5V dc., is the ICG crystal oscillator supposed to run? Always/ sometimes/ never?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards, Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jul 2012 04:54:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-oscillator-operation/m-p/179129#M12809</guid>
      <dc:creator>BobMac</dc:creator>
      <dc:date>2012-07-13T04:54:19Z</dc:date>
    </item>
    <item>
      <title>Re: ICG oscillator operation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-oscillator-operation/m-p/179130#M12810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bob,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After POR, the default operating mode for the ICG module will be FEI.&amp;nbsp; The crystal oscillator will be inoperative.&amp;nbsp; You will then&amp;nbsp;need to set ICGC1 to enable the oscillator, and to switch to FEE mode.&amp;nbsp; Refer to the datasheet, section 10.5.3, Example #2 for the required procedure.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jul 2012 13:00:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICG-oscillator-operation/m-p/179130#M12810</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-07-13T13:00:19Z</dc:date>
    </item>
  </channel>
</rss>