<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックUrgent need for help. Non volatile MC13213 application parameters.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/178998#M12782</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I'm developing an SMAC application for the MC13213 device. I would need to store some parameters (approx 10-16 bytes) to non volatile flash memory. This must be done from the application code itself (on a daily basis at maximum).&lt;BR /&gt;&lt;BR /&gt;I have seen suggestions for how to achieve this in a Freescale forum thread. See S08_Flash_A2.zip attached to a post in the forum thread for the suggested solution.&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fmessage%2F68186%2368186" rel="nofollow" target="_blank"&gt;https://community.freescale.com/message/68186#68186&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;However I don't know what changes must be done to my PRM file.&lt;BR /&gt;&lt;BR /&gt;I have attached the PRM file of my project. I would be most grateful if I could assistance with the appropriate changes of my PRM file.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;&lt;BR /&gt;Johan Hammar&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jan 2011 02:08:58 GMT</pubDate>
    <dc:creator>Jonte</dc:creator>
    <dc:date>2011-01-26T02:08:58Z</dc:date>
    <item>
      <title>Urgent need for help. Non volatile MC13213 application parameters.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/178998#M12782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I'm developing an SMAC application for the MC13213 device. I would need to store some parameters (approx 10-16 bytes) to non volatile flash memory. This must be done from the application code itself (on a daily basis at maximum).&lt;BR /&gt;&lt;BR /&gt;I have seen suggestions for how to achieve this in a Freescale forum thread. See S08_Flash_A2.zip attached to a post in the forum thread for the suggested solution.&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fmessage%2F68186%2368186" rel="nofollow" target="_blank"&gt;https://community.freescale.com/message/68186#68186&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;However I don't know what changes must be done to my PRM file.&lt;BR /&gt;&lt;BR /&gt;I have attached the PRM file of my project. I would be most grateful if I could assistance with the appropriate changes of my PRM file.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;&lt;BR /&gt;Johan Hammar&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jan 2011 02:08:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/178998#M12782</guid>
      <dc:creator>Jonte</dc:creator>
      <dc:date>2011-01-26T02:08:58Z</dc:date>
    </item>
    <item>
      <title>Re: Urgent need for help. Non volatile MC13213 application parameters.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/178999#M12783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Johan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You initially had some problems with overlapping or segments with incorrect range.&amp;nbsp; These needed to be first corrected, before making the changes required to place the RAM based code.&amp;nbsp; These corrections are shown in red, within the following PRM.&amp;nbsp; I have also re-sequenced some ot the lines for clarity, but should not affect PRM operation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/* Linker parameter file for the GB60 */NAMESENDSECTIONS /* all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */  Z_RAM        = READ_WRITE 0x0080 TO 0x00FF;   RAM          = READ_WRITE 0x0100 TO &lt;FONT color="#0000ff"&gt;0x0B7F&lt;/FONT&gt;; //0x107F;  Adjust to allow for SSTACK  &lt;FONT color="#0000ff"&gt;SSTACK       = READ_WRITE 0x0B80 TO 0x107F; // Explicit stack section now defined.&lt;/FONT&gt;  ROM2         = READ_ONLY  0x1080 TO &lt;FONT color="#0000ff"&gt;0x13EF&lt;/FONT&gt;; //&lt;FONT color="#ff0000"&gt;0x17FF;  Previous overlap with NVRAM&lt;/FONT&gt;  &lt;FONT color="#0000ff"&gt;FLASH_TO_RAM = READ_ONLY  0x13F0 TO 0x13FF RELOCATE TO 0x0B80; // RAM based code.&lt;/FONT&gt;  NVRAM        = NO_INIT    0x1400 TO 0x17FF; //&lt;FONT color="#ff0000"&gt;0x1800&lt;/FONT&gt;; /* 802.15.4 MAC NVRAM AREA */  ROM          = READ_ONLY  0x182C TO 0xFAFF; //&lt;FONT color="#ff0000"&gt;0xFEFF;  Previous overlap with vector area&lt;/FONT&gt;ENDPLACEMENT /* all predefined and user segments are placed into the SECTIONS defined above. */  _DATA_ZEROPAGE, MY_ZEROPAGE   INTO Z_RAM;  DEFAULT_RAM                   INTO RAM;  DEFAULT_ROM                   INTO ROM/*, ROM2*/;   /* in case you want to use ROM2 here as well, add option -OnB=b to the compiler. */  DOT4MAC_NVRAM                 INTO NVRAM;  &lt;FONT color="#0000ff"&gt;FLASH_ROUTINE                 INTO FLASH_TO_RAM;&lt;/FONT&gt; END&lt;FONT color="#0000ff"&gt;STACKTOP 0x107F&lt;/FONT&gt;//STACKSIZE 0x500          VECTOR 0 _Startup /* reset vector: default entry point for a C/C++ application. */&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The additional and modified items, for flash programming purposes, are shown in blue.&amp;nbsp; The intent is to place the code that is eventually&amp;nbsp;relocated RAM (bottom of&amp;nbsp;stack&amp;nbsp;position)&amp;nbsp;at&amp;nbsp;the&amp;nbsp;FLASH_TO_RAM location.&amp;nbsp; A stack segment SSEG is also explicitly defined&amp;nbsp;so that the bottom of&amp;nbsp;stack position is known.&amp;nbsp; Consequently, STACKTOP (rather than STACKSIZE) has been defined.&amp;nbsp; The size of the stack should remain at 0x500 bytes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When modifying a PRM, make sure that the various sections that are defined do not overlap each other.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/178999#M12783</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2020-10-29T09:28:14Z</dc:date>
    </item>
    <item>
      <title>Re: Urgent need for help. Non volatile MC13213 application parameters.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179000#M12784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mac,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your promt reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately I get the following Linker error when attempting to build my codewarrior project using the corrected PRM file that you provided:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error: L1004: ';' expected&lt;/P&gt;&lt;P&gt;Linker.prm line 11&lt;/P&gt;&lt;P&gt;Linker Error: Link failed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(This is the line defining the FLASH_TO_RAM section).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Johan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jan 2011 23:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179000#M12784</guid>
      <dc:creator>Jonte</dc:creator>
      <dc:date>2011-01-27T23:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: Urgent need for help. Non volatile MC13213 application parameters.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179001#M12785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Apparently you are looking for a way to run portion of your application from the stack.&lt;/P&gt;&lt;P&gt;If this is what you intend to do, refer to attached Technical note.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You cannot use RELOCATE?TO in that particular case.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jan 2011 23:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179001#M12785</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2011-01-27T23:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: Urgent need for help. Non volatile MC13213 application parameters.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179002#M12786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The method of flash programming that the OP refers is &lt;U&gt;not&lt;/U&gt; of the "do_on_stack" variety, which I think TN235 refers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The method being attempted actually uses a 16 byte block of code that needs to be relocated to a fixed position in RAM, and executed.&amp;nbsp; It so happens that the RAM position being attempted is the very bottom of the stack segment, where it will least likely be disturbed by normal stack operations, in the short term at least.&amp;nbsp; However, any other suitable block of RAM could have been used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not sure of the reason for the L1004 error - it seems to be indicating a missing semi-colon - but this method of relocation has previously been&amp;nbsp;successfully used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jan 2011 03:11:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179002#M12786</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-01-28T03:11:30Z</dc:date>
    </item>
    <item>
      <title>Re: Urgent need for help. Non volatile MC13213 application parameters.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179003#M12787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is a little typo in the prm on line 11. The line contains the two words RELOCATE TO, but actually the linker expects &amp;nbsp;RELOCATE_TO, a single keyword with an underscore.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jan 2011 14:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Urgent-need-for-help-Non-volatile-MC13213-application-parameters/m-p/179003#M12787</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2011-01-28T14:56:01Z</dc:date>
    </item>
  </channel>
</rss>