<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Questions about S08ICSV3 (MC9S08QEx) Clock Generator in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177882#M12598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wingsy,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is that the DMX32 = 1 setting is intended for use with an external 32.768kHz crystal reference, because of the proximity to the&amp;nbsp;DCO upper frequency limit (with the increased multiplying factor).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When using the internal reference, I would tend to use DMX32 = 0 setting. so that the DCO frequency will remain within its operating range, even prior to the reference being trimmed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Oct 2011 21:20:21 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2011-10-28T21:20:21Z</dc:date>
    <item>
      <title>Questions about S08ICSV3 (MC9S08QEx) Clock Generator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177881#M12597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My objective is to get a fast stable BUSCLK (internal osc) from a QE8 as simple as possible. This is what I've read in AN3499 (Clock Options on the HC9S08 Family) about the ICS in section 2.1:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Table 4 shows that with DRS bits = 00 and DMX32=1 that I get a reference freq of 32.768K and a DCO output freq of 19.92M, which can give me a BUSCLK of 9.96M. It also states in section 2.1.5.4 (about the ICS Status &amp;amp; Control reg) that&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"The register also contains the DCO maximum frequency bit (DMX32) that determines if a finely tuned reference frequency of 32.768 kHz is used. When using this reference, the DCO multipliers are greater when compared to general reference frequencies and this provides a fixed DCO output."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 14px;"&gt;When I read "a finely tuned reference frequency..." it made me wonder WHO does this "finely tuned" thing, me via the trim bits, or Freescale in the chip? Table 4 makes me think it is independant of the trim bits.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 14px;"&gt;Anyone have any experience using it this way?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2011 17:26:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177881#M12597</guid>
      <dc:creator>Wingsy</dc:creator>
      <dc:date>2011-10-28T17:26:48Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about S08ICSV3 (MC9S08QEx) Clock Generator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177882#M12598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Wingsy,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is that the DMX32 = 1 setting is intended for use with an external 32.768kHz crystal reference, because of the proximity to the&amp;nbsp;DCO upper frequency limit (with the increased multiplying factor).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When using the internal reference, I would tend to use DMX32 = 0 setting. so that the DCO frequency will remain within its operating range, even prior to the reference being trimmed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Oct 2011 21:20:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177882#M12598</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-10-28T21:20:21Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about S08ICSV3 (MC9S08QEx) Clock Generator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177883#M12599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What BigMac is saying is correct...if you set DMX32=1 and use the internal oscillator you could violate timing requirements if the internal oscillator is trimmed&amp;nbsp;higher than 32768Hz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Oct 2011 03:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177883#M12599</guid>
      <dc:creator>PG1</dc:creator>
      <dc:date>2011-10-29T03:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about S08ICSV3 (MC9S08QEx) Clock Generator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177884#M12600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks you two.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Oct 2011 00:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Questions-about-S08ICSV3-MC9S08QEx-Clock-Generator/m-p/177884#M12600</guid>
      <dc:creator>Wingsy</dc:creator>
      <dc:date>2011-10-30T00:03:39Z</dc:date>
    </item>
  </channel>
</rss>