<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: about RTI,I need an example-urgent_MC13213</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177428#M12517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi bigmac :&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; Thanks for your help!&lt;BR /&gt;&amp;nbsp; I'm sorry that the above description is not clear enough!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; It's sure that I don't konw how to set up the RTI module for generating a RTI interrupt,such as the SRTISC register or need other registers!&lt;BR /&gt;&amp;nbsp; The following code is a small test program,compiler under the CW6.1 and MC13213.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;#include &amp;lt;hidef.h&amp;gt;&lt;BR /&gt;#include "derivative.h"&lt;/DIV&gt;&lt;DIV&gt;void Init_RTI(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;SRTISC=0xff;&amp;nbsp; //set up the SRTISC register,how to config it?&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;void Init_IO()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;PTDD_PTDD4 = 1;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;PTDDD_PTDDD4=1; //output,for lighting a led&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;void main(void) {&lt;BR /&gt;&amp;nbsp; Init_RTI();&lt;BR /&gt;&amp;nbsp; Init_IO();&lt;BR /&gt;&amp;nbsp; EnableInterrupts;&lt;BR /&gt;&amp;nbsp; for( ; ; )&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __RESET_WATCHDOG();&lt;BR /&gt;&amp;nbsp; }&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;interrupt VectorNumber_Vrti void RTI_ISR(void)&amp;nbsp; //RTI interrupt,but cann't be trigger here,WHY?&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; if((SRTISC&amp;amp;0x80)==0x80){&lt;BR /&gt;&amp;nbsp; &amp;nbsp;SRTISC_RTIACK=1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //clear&lt;BR /&gt;&amp;nbsp; &amp;nbsp;PTDD_PTDD4=~PTDD_PTDD4;&amp;nbsp; //on or off&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Running it,but the led was never lighted,I think the RTI module initializtion is wrong!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Please give me some hints!&lt;/DIV&gt;&lt;DIV&gt;Thanks again.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Best regards,&lt;BR /&gt;Charly&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Beijing2008 on &lt;SPAN class="date_text"&gt;2008-07-31&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;04:47 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Jul 2008 10:44:34 GMT</pubDate>
    <dc:creator>Beijing2008</dc:creator>
    <dc:date>2008-07-31T10:44:34Z</dc:date>
    <item>
      <title>about RTI,I need an example-urgent_MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177426#M12515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi all:&lt;/DIV&gt;&lt;DIV&gt;I'm using MC13213 and CW6.1,Now I would like to generate a timer,trigger a timer interrupt per N*second.&lt;/DIV&gt;&lt;DIV&gt;how to use the RTI(real-time interrupt)? please give me an simple example!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks and best regards,&lt;BR /&gt;Charly&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2008 08:15:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177426#M12515</guid>
      <dc:creator>Beijing2008</dc:creator>
      <dc:date>2008-07-31T08:15:48Z</dc:date>
    </item>
    <item>
      <title>Re: about RTI,I need an example-urgent_MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177427#M12516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Charly,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I will assume that you have set up the RTI module to generate an interrupt once per second.&amp;nbsp; Then your ISR&amp;nbsp;might contain the following code -&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New"&gt;if (tcounter) {&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New"&gt;&amp;nbsp;&amp;nbsp; tcounter--;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New"&gt;&amp;nbsp;&amp;nbsp; if (!tcounter) {&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Do timeout action here&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New"&gt;&amp;nbsp;&amp;nbsp; }&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New"&gt;}&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;where &lt;FONT face="Courier New"&gt;tcounter&lt;/FONT&gt; is a global variable of a suitable size.&amp;nbsp; To commence a timeout period, set the value of &lt;FONT face="Courier New"&gt;tcounter&lt;/FONT&gt; to the number of seconds required.&amp;nbsp; If the action required on timeout is too time consuming to be included within the ISR, you would need to poll for the occurrence of timeout - simply test whether the global variable has reached a value of zero.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2008 09:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177427#M12516</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-07-31T09:24:05Z</dc:date>
    </item>
    <item>
      <title>Re: about RTI,I need an example-urgent_MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177428#M12517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hi bigmac :&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; Thanks for your help!&lt;BR /&gt;&amp;nbsp; I'm sorry that the above description is not clear enough!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; It's sure that I don't konw how to set up the RTI module for generating a RTI interrupt,such as the SRTISC register or need other registers!&lt;BR /&gt;&amp;nbsp; The following code is a small test program,compiler under the CW6.1 and MC13213.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;#include &amp;lt;hidef.h&amp;gt;&lt;BR /&gt;#include "derivative.h"&lt;/DIV&gt;&lt;DIV&gt;void Init_RTI(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;SRTISC=0xff;&amp;nbsp; //set up the SRTISC register,how to config it?&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;void Init_IO()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;PTDD_PTDD4 = 1;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; &amp;nbsp;PTDDD_PTDDD4=1; //output,for lighting a led&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;void main(void) {&lt;BR /&gt;&amp;nbsp; Init_RTI();&lt;BR /&gt;&amp;nbsp; Init_IO();&lt;BR /&gt;&amp;nbsp; EnableInterrupts;&lt;BR /&gt;&amp;nbsp; for( ; ; )&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __RESET_WATCHDOG();&lt;BR /&gt;&amp;nbsp; }&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;interrupt VectorNumber_Vrti void RTI_ISR(void)&amp;nbsp; //RTI interrupt,but cann't be trigger here,WHY?&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; if((SRTISC&amp;amp;0x80)==0x80){&lt;BR /&gt;&amp;nbsp; &amp;nbsp;SRTISC_RTIACK=1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //clear&lt;BR /&gt;&amp;nbsp; &amp;nbsp;PTDD_PTDD4=~PTDD_PTDD4;&amp;nbsp; //on or off&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;}&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Running it,but the led was never lighted,I think the RTI module initializtion is wrong!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Please give me some hints!&lt;/DIV&gt;&lt;DIV&gt;Thanks again.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Best regards,&lt;BR /&gt;Charly&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Beijing2008 on &lt;SPAN class="date_text"&gt;2008-07-31&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;04:47 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2008 10:44:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177428#M12517</guid>
      <dc:creator>Beijing2008</dc:creator>
      <dc:date>2008-07-31T10:44:34Z</dc:date>
    </item>
    <item>
      <title>Re: about RTI,I need an example-urgent_MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177429#M12518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Charly,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It is possible that you do not have the correct RTI clock source selected, and this will depend on the operating mode when RTI operation is required.&amp;nbsp; According to the datasheet, there are the following restrictions for the clock source -&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Run mode - External reference clock only&lt;/DIV&gt;&lt;DIV&gt;Wait mode - External reference clock only&lt;/DIV&gt;&lt;DIV&gt;Stop3 - Either clock source&lt;/DIV&gt;&lt;DIV&gt;Stop2 - Internal RTI clock only&lt;/DIV&gt;&lt;DIV&gt;Stop1 - RTI inoperative&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Assuming your tests use run mode, you will need to provide an external reference signal, and set the control bit SRTISC_RTICLKS.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Aug 2008 09:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/about-RTI-I-need-an-example-urgent-MC13213/m-p/177429#M12518</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-08-01T09:15:39Z</dc:date>
    </item>
  </channel>
</rss>