<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08MP16 KBI problem in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08MP16-KBI-problem/m-p/176407#M12305</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have to checked for the polarity for interrupt event though this should not be a problem?&lt;/P&gt;&lt;P&gt;Have you acitivated pull-up resistor for that particular pin provided you are not using external pull up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jul 2012 12:20:47 GMT</pubDate>
    <dc:creator>sandeepnaik</dc:creator>
    <dc:date>2012-07-10T12:20:47Z</dc:date>
    <item>
      <title>MC9S08MP16 KBI problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08MP16-KBI-problem/m-p/176406#M12304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;Nowadays, i have some problem in Keyboard Interrupt function of MC9S08MP16.&lt;/P&gt;&lt;P&gt;The Port is PTD4/KBI3P4/PDB2OUT that is connected Hall effect sensor(open collector type).&lt;/P&gt;&lt;P&gt;also the &lt;SPAN&gt;Hall effect sensor input is connected to FTMCH1(to use as input capture function).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;the problem is.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;- Port value is changed in debug mode well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;- but, there's no KBI event.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;( I already checked KBI Function by using push button switch so many times.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I confirm, KBI initialize and setup are no problem..)&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;- &lt;SPAN&gt;input capture interrupt is running well.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder, Input capture interrupt well,,,,, but KBI no event?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope your advice..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a nice day~&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Jul 2012 18:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08MP16-KBI-problem/m-p/176406#M12304</guid>
      <dc:creator>Maximus_KR</dc:creator>
      <dc:date>2012-07-01T18:35:20Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08MP16 KBI problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08MP16-KBI-problem/m-p/176407#M12305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have to checked for the polarity for interrupt event though this should not be a problem?&lt;/P&gt;&lt;P&gt;Have you acitivated pull-up resistor for that particular pin provided you are not using external pull up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2012 12:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08MP16-KBI-problem/m-p/176407#M12305</guid>
      <dc:creator>sandeepnaik</dc:creator>
      <dc:date>2012-07-10T12:20:47Z</dc:date>
    </item>
  </channel>
</rss>