<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic is address map built automatically? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/is-address-map-built-automatically/m-p/176068#M12283</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi all&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I know that address map is automatically built in coordinator when each node joins the network.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this true for end devices and routers?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to built address map for every node in the network so that it holds specific nodes addresses.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;have I do it myself or the address map is built automatically in end devices?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I have to built it, when should I use addr_req for example?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;THANKS&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Jul 2008 17:54:37 GMT</pubDate>
    <dc:creator>bitasobhani</dc:creator>
    <dc:date>2008-07-28T17:54:37Z</dc:date>
    <item>
      <title>is address map built automatically?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/is-address-map-built-automatically/m-p/176068#M12283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi all&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I know that address map is automatically built in coordinator when each node joins the network.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is this true for end devices and routers?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need to built address map for every node in the network so that it holds specific nodes addresses.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;have I do it myself or the address map is built automatically in end devices?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If I have to built it, when should I use addr_req for example?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;THANKS&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2008 17:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/is-address-map-built-automatically/m-p/176068#M12283</guid>
      <dc:creator>bitasobhani</dc:creator>
      <dc:date>2008-07-28T17:54:37Z</dc:date>
    </item>
    <item>
      <title>Re: is address map built automatically?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/is-address-map-built-automatically/m-p/176069#M12284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;the Address Map can be filled in several ways. But the most important "trigger" is the ieee_addr_req and nwk_addr_req.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;when the responses is received the address map is filled out, so you e.g.&amp;nbsp; can communicate on a 64 bit address.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Br,&lt;/DIV&gt;&lt;DIV&gt;Mads&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2008 23:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/is-address-map-built-automatically/m-p/176069#M12284</guid>
      <dc:creator>Mads</dc:creator>
      <dc:date>2008-08-05T23:07:54Z</dc:date>
    </item>
  </channel>
</rss>