<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Demo QE board and BDM in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Demo-QE-board-and-BDM/m-p/175485#M12192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Add the 6 pin header, get a 6 pin IDC cable, and you are ready to rock.&lt;BR /&gt;&lt;BR /&gt;It is a a full P&amp;amp;E BDM and will work with CFV1, S08 and S(X)12 boards.&lt;BR /&gt;&lt;BR /&gt;However, do not expect it to supply power to the board. I have been told it is also not as well protected and a USB 12 is - not sure what that means.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Dec 2007 01:25:26 GMT</pubDate>
    <dc:creator>JimDon</dc:creator>
    <dc:date>2007-12-29T01:25:26Z</dc:date>
    <item>
      <title>Demo QE board and BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Demo-QE-board-and-BDM/m-p/175484#M12191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is: can I use the Demo QE board's BDM to program any other S08 or S12X? Or is it limited to flexis microcontrolers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mav&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2007 21:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Demo-QE-board-and-BDM/m-p/175484#M12191</guid>
      <dc:creator>maverick</dc:creator>
      <dc:date>2007-12-28T21:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: Demo QE board and BDM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Demo-QE-board-and-BDM/m-p/175485#M12192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Add the 6 pin header, get a 6 pin IDC cable, and you are ready to rock.&lt;BR /&gt;&lt;BR /&gt;It is a a full P&amp;amp;E BDM and will work with CFV1, S08 and S(X)12 boards.&lt;BR /&gt;&lt;BR /&gt;However, do not expect it to supply power to the board. I have been told it is also not as well protected and a USB 12 is - not sure what that means.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Dec 2007 01:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Demo-QE-board-and-BDM/m-p/175485#M12192</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2007-12-29T01:25:26Z</dc:date>
    </item>
  </channel>
</rss>