<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMagnetometers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Magnetometers/m-p/175136#M12151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not surprisingly there's not a forum called 'Magnetometers' so I hope I'll be forgiven for posting here instead.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll be using the MAG3110 magnetometer in a surveying application.&amp;nbsp; This application will use the magnetometer to find compass heading from the earth's magnetic field.&amp;nbsp; To get the best accuracy the sensor should not have any ferromagnetic materials nearby.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is how diligent do I have to be in keeping magnetic components off&amp;nbsp; the circuit board?&amp;nbsp; If I'm forced to use them then how far away do they have to be from the sensor to minimise their influence?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've source non-magnetic resistors and capacitors as well as a low magnetic signature battery.&amp;nbsp; But non-magnetic crystal oscillators seem less common.&amp;nbsp; I don't want to spend lots of dollars and time on sourcing non-magnetic components unless there is a real benefit, but I don't know how to quantify that benefit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jun 2012 09:34:46 GMT</pubDate>
    <dc:creator>DGN</dc:creator>
    <dc:date>2012-06-26T09:34:46Z</dc:date>
    <item>
      <title>Magnetometers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Magnetometers/m-p/175136#M12151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not surprisingly there's not a forum called 'Magnetometers' so I hope I'll be forgiven for posting here instead.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll be using the MAG3110 magnetometer in a surveying application.&amp;nbsp; This application will use the magnetometer to find compass heading from the earth's magnetic field.&amp;nbsp; To get the best accuracy the sensor should not have any ferromagnetic materials nearby.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is how diligent do I have to be in keeping magnetic components off&amp;nbsp; the circuit board?&amp;nbsp; If I'm forced to use them then how far away do they have to be from the sensor to minimise their influence?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've source non-magnetic resistors and capacitors as well as a low magnetic signature battery.&amp;nbsp; But non-magnetic crystal oscillators seem less common.&amp;nbsp; I don't want to spend lots of dollars and time on sourcing non-magnetic components unless there is a real benefit, but I don't know how to quantify that benefit.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2012 09:34:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Magnetometers/m-p/175136#M12151</guid>
      <dc:creator>DGN</dc:creator>
      <dc:date>2012-06-26T09:34:46Z</dc:date>
    </item>
    <item>
      <title>Re: Magnetometers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Magnetometers/m-p/175137#M12152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When choosing components I would try to avoid those using ferromagnetic materials.&amp;nbsp; However, I would not have thought that standard SM resistors and capacitors would have been an issue.&amp;nbsp; Do you really need to use a crystal?&amp;nbsp; Can you make use of the internal reference within the MCU (assuming a MC9S08 MCU type)?&amp;nbsp; If you need an accurate bus frequency, perhaps the use of a low frequency watch crystal would be better than a higher frequency crystal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think that you will ultimately need to experiment with the placement of any suspect components, to test their effect on the 3-axis measurement.&amp;nbsp; I would certainly check the intended battery placement.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another consideration might be the placement of PCB tracks in the vicinity of the sensor, especially for those carrying any significant&amp;nbsp;current.&amp;nbsp;&amp;nbsp;I guess there&amp;nbsp;should not be any&amp;nbsp;of these&amp;nbsp;tracks&amp;nbsp;immediately below the sensor.&amp;nbsp; For a PCB track that passes the sensor at a distance of 10mm, the flux density at the sensor position caused by the track current would be about 0.02uT per mA, using the formula&amp;nbsp;&lt;FONT face="courier new,courier"&gt;B = u0*I /(2*pi*d)&lt;FONT face="arial,helvetica,sans-serif"&gt;.&amp;nbsp;&lt;/FONT&gt;&lt;/FONT&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;&amp;nbsp;&lt;/FONT&gt;Compare this with the sensor sensitivity of 0.1uT per LSB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2012 23:29:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Magnetometers/m-p/175137#M12152</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-06-26T23:29:44Z</dc:date>
    </item>
  </channel>
</rss>