<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: USB BDM Multilink for HCS08</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175134#M12149</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need advice on how to use the USB BDM Multilink for flashing code into microcontroller. I did it this way:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- In CodeWarrior IDE, do whatever code changes as necessary. Then 'Project -&amp;gt; Make' to compile the code&lt;/P&gt;&lt;P&gt;- Click the 'Debug' buttor to bring up the True-Time Simulator &amp;amp; Real-Time Debugger&lt;/P&gt;&lt;P&gt;- Make sure the Berg connector is already plugged in, and powered on&lt;/P&gt;&lt;P&gt;- In the PEMICRO Connection Manager, click 'Connect (Reset)'. The BDM Multilink should be connected to the microcontroller now&lt;/P&gt;&lt;P&gt;- Click 'No' on the 'Erase and Program Flash?' dialog box&lt;/P&gt;&lt;P&gt;- In the True-Time Simulator window, 'File -&amp;gt; Load Application..' and choose the *.abs file to load&lt;/P&gt;&lt;P&gt;- Click 'Yes' on the 'Erase and Program Flash?' dialog box&lt;/P&gt;&lt;P&gt;- The code should be flashed successfully into the microcontroller&lt;/P&gt;&lt;P&gt;- Click the 'Start/Continue (F5)' green icon to start running the code and debugging&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this the right process?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Jan 2011 15:44:52 GMT</pubDate>
    <dc:creator>leesp</dc:creator>
    <dc:date>2011-01-31T15:44:52Z</dc:date>
    <item>
      <title>USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175128#M12143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to do debugging &amp;amp; flashing of code to MC9S08JM32.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I noted that there is a USD99 USB BDM Multilink from P&amp;amp;E Micro. My question is:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;- Do I need to purchase other software in order to be able to do background debugging and flashing of code using the Multilink?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I already have CodeWarrior for Microcontroller.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jan 2011 13:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175128#M12143</guid>
      <dc:creator>leesp</dc:creator>
      <dc:date>2011-01-11T13:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175129#M12144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;No. All the required software is included with Codewarrior.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jan 2011 15:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175129#M12144</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2011-01-11T15:53:42Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175130#M12145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peg,&lt;/P&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;Assuming I plugged in the USB Multilink now, what do I need to do with CodeWarrior? I mean how do I start the flashing operation? I search "flash commands" in the CodeWarrior Help but couldn't find how to quick start.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jan 2011 17:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175130#M12145</guid>
      <dc:creator>leesp</dc:creator>
      <dc:date>2011-01-11T17:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175131#M12146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using CodeWarrior's True-Time Simulator &amp;amp; Real-Time Debugger with PEMicro USB BDM Multilink to flash code and debug.&lt;/P&gt;&lt;P&gt;On the True-Time Simulator's "Memory" window, what should I do so that I could see real time refresh of a memory variable? I mean in my code, as it runs, a variable keeps changing. But I have to right-click on the Memory window and do a "Refresh" in order to see how the variable changes.&lt;/P&gt;&lt;P&gt;Can't it refresh automatically?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jan 2011 15:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175131#M12146</guid>
      <dc:creator>leesp</dc:creator>
      <dc:date>2011-01-28T15:44:16Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175132#M12147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not a user of Codewarrior, but I believe there is an option to "update on halt" or something like that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jan 2011 16:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175132#M12147</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2011-01-28T16:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175133#M12148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the memory and watch windows you can right click and set the mode to 'Periodic' and select the refresh rate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jan 2011 22:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175133#M12148</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-01-28T22:09:39Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175134#M12149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need advice on how to use the USB BDM Multilink for flashing code into microcontroller. I did it this way:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- In CodeWarrior IDE, do whatever code changes as necessary. Then 'Project -&amp;gt; Make' to compile the code&lt;/P&gt;&lt;P&gt;- Click the 'Debug' buttor to bring up the True-Time Simulator &amp;amp; Real-Time Debugger&lt;/P&gt;&lt;P&gt;- Make sure the Berg connector is already plugged in, and powered on&lt;/P&gt;&lt;P&gt;- In the PEMICRO Connection Manager, click 'Connect (Reset)'. The BDM Multilink should be connected to the microcontroller now&lt;/P&gt;&lt;P&gt;- Click 'No' on the 'Erase and Program Flash?' dialog box&lt;/P&gt;&lt;P&gt;- In the True-Time Simulator window, 'File -&amp;gt; Load Application..' and choose the *.abs file to load&lt;/P&gt;&lt;P&gt;- Click 'Yes' on the 'Erase and Program Flash?' dialog box&lt;/P&gt;&lt;P&gt;- The code should be flashed successfully into the microcontroller&lt;/P&gt;&lt;P&gt;- Click the 'Start/Continue (F5)' green icon to start running the code and debugging&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this the right process?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jan 2011 15:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175134#M12149</guid>
      <dc:creator>leesp</dc:creator>
      <dc:date>2011-01-31T15:44:52Z</dc:date>
    </item>
    <item>
      <title>Re: USB BDM Multilink for HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175135#M12150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You should be able to leave out your steps 5 &amp;amp; 6 IIRC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jan 2011 18:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-BDM-Multilink-for-HCS08/m-p/175135#M12150</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2011-01-31T18:15:29Z</dc:date>
    </item>
  </channel>
</rss>