<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCHC908QY1CDW versus MC68HC908QY1CDW in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174766#M12086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;dsweeney@gtdev.com wrote:&lt;BR /&gt;&lt;P&gt;The markings on the chip it's self are missing the 68 and I want to know what changed?&amp;nbsp; Are you saying that the parts marked MCHC908QY1CDW are in fact the newer version QY1A's?&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I have seen package markings with&amp;nbsp;'MC68HC908'&amp;nbsp;and with 'MC908', but I have not previously seen the marking 'MCHC908'.&amp;nbsp; An A-suffix&amp;nbsp;device should&amp;nbsp;have its package&amp;nbsp;marked with the 'A' suffix, i.e. MC908QY1ACDW or MC908QY1ACDWE for lead-free package.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jun 2012 22:12:07 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2012-06-26T22:12:07Z</dc:date>
    <item>
      <title>MCHC908QY1CDW versus MC68HC908QY1CDW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174762#M12082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was hoping that someone could tell me what the diffrence is between parts marked with MC68CH908.... and MCHC908... are?&amp;nbsp; The parts without the "68" are programmed correctly and the ones with&amp;nbsp;the 68 seem to be all over the place with operation in our assemblies.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jun 2012 06:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174762#M12082</guid>
      <dc:creator>dsweeney</dc:creator>
      <dc:date>2012-06-23T06:40:02Z</dc:date>
    </item>
    <item>
      <title>Re: MCHC908QY1CDW versus MC68HC908QY1CDW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174763#M12083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You have actually placed this post in the wrong forum - the device that you refer is 8-bits.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When the part was first introduced, the full part number was MC68HC908QY1, with the following suffix letters representing the temperature range and package type.&amp;nbsp; There was also another version, the&amp;nbsp;MC68HLC908QY1 that had some electrical differences.&lt;/P&gt;&lt;P&gt;Sometime later, an enhanced version was introduced, the MC68HC908QY1A (or A-suffix version).&lt;/P&gt;&lt;P&gt;Then subsequently Freescale dropped the "68HC" within&amp;nbsp;all part numbers, without any other documented changes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MC908QY1 is equivalent to MC68HC908QY1&lt;/P&gt;&lt;P&gt;MCL908YY1 is equivalent to MC68HLC908QY1&lt;/P&gt;&lt;P&gt;MC908QY1A is equivalent to MC68HC908QY1A&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is&amp;nbsp;quite likely that code developed for the earlier device will still work on the A-suffix version.&amp;nbsp; However, It is&amp;nbsp;possible that the code developed for the A-suffix version may not work properly on&amp;nbsp;the earlier device, depending on whether any of the&amp;nbsp;modified features are used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2012 22:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174763#M12083</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-06-25T22:40:02Z</dc:date>
    </item>
    <item>
      <title>Re: MCHC908QY1CDW versus MC68HC908QY1CDW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174764#M12084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for the response Bigmac!&amp;nbsp; Sorry for the 8bit and 16 bit confusion.&amp;nbsp; I think I need to be clearer on where the markings are...&amp;nbsp; The markings on the chip it's self are missing the 68 and I want to know what changed?&amp;nbsp; Are you saying that the parts marked MCHC908QY1CDW are in fact the newer version QY1A's?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2012 02:25:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174764#M12084</guid>
      <dc:creator>dsweeney</dc:creator>
      <dc:date>2012-06-26T02:25:54Z</dc:date>
    </item>
    <item>
      <title>Re: MCHC908QY1CDW versus MC68HC908QY1CDW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174765#M12085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale never types out 68 on the markings for the QY, like they do for some other 68HC08 parts.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why? Because Freescale just love inconsistent chip markings. I don't think there exists a single Freescale chip with a printed partnumber on it, that is 100% corresponding to the documentation in the manual/erratas.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2012 19:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174765#M12085</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2012-06-26T19:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: MCHC908QY1CDW versus MC68HC908QY1CDW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174766#M12086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;dsweeney@gtdev.com wrote:&lt;BR /&gt;&lt;P&gt;The markings on the chip it's self are missing the 68 and I want to know what changed?&amp;nbsp; Are you saying that the parts marked MCHC908QY1CDW are in fact the newer version QY1A's?&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I have seen package markings with&amp;nbsp;'MC68HC908'&amp;nbsp;and with 'MC908', but I have not previously seen the marking 'MCHC908'.&amp;nbsp; An A-suffix&amp;nbsp;device should&amp;nbsp;have its package&amp;nbsp;marked with the 'A' suffix, i.e. MC908QY1ACDW or MC908QY1ACDWE for lead-free package.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2012 22:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCHC908QY1CDW-versus-MC68HC908QY1CDW/m-p/174766#M12086</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-06-26T22:12:07Z</dc:date>
    </item>
  </channel>
</rss>