<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックQG8 on USBSPYDER Problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-on-USBSPYDER-Problem/m-p/174484#M12053</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on&amp;nbsp; a Universal infrared receiver using QG8.&lt;BR /&gt;&lt;BR /&gt;As VCC i have dropped 5V to 3.6V using 2 diodes in series. The output pin PTAD1 drives&amp;nbsp; a relay through a transistor.&lt;BR /&gt;&lt;BR /&gt;The transistor turns on when the code is run through USBSPYDER and subsequently turns OFF also, as intended. But when i connect my circuit to independent 3.6V(which i generate from 5V), the transistor turns ON but it never responds after that. Is this something related to RESET? i have disabled COP.&lt;BR /&gt;&lt;BR /&gt;Kindly help me as always.&lt;BR /&gt;&lt;BR /&gt;Thanks and Regards,&lt;BR /&gt;Ameya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Apr 2009 22:05:14 GMT</pubDate>
    <dc:creator>Amey</dc:creator>
    <dc:date>2009-04-22T22:05:14Z</dc:date>
    <item>
      <title>QG8 on USBSPYDER Problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-on-USBSPYDER-Problem/m-p/174484#M12053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working on&amp;nbsp; a Universal infrared receiver using QG8.&lt;BR /&gt;&lt;BR /&gt;As VCC i have dropped 5V to 3.6V using 2 diodes in series. The output pin PTAD1 drives&amp;nbsp; a relay through a transistor.&lt;BR /&gt;&lt;BR /&gt;The transistor turns on when the code is run through USBSPYDER and subsequently turns OFF also, as intended. But when i connect my circuit to independent 3.6V(which i generate from 5V), the transistor turns ON but it never responds after that. Is this something related to RESET? i have disabled COP.&lt;BR /&gt;&lt;BR /&gt;Kindly help me as always.&lt;BR /&gt;&lt;BR /&gt;Thanks and Regards,&lt;BR /&gt;Ameya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2009 22:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-on-USBSPYDER-Problem/m-p/174484#M12053</guid>
      <dc:creator>Amey</dc:creator>
      <dc:date>2009-04-22T22:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 on USBSPYDER Problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-on-USBSPYDER-Problem/m-p/174485#M12054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You should try to use a voltage regulator instead of series diodes (e.g. fixed 3.6 volt output, low drop, like LP2981).&lt;/P&gt;&lt;P&gt;Please write again, if problem persists.&lt;/P&gt;&lt;P&gt;Klaus&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2009 22:21:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-on-USBSPYDER-Problem/m-p/174485#M12054</guid>
      <dc:creator>Problem99</dc:creator>
      <dc:date>2009-05-07T22:21:09Z</dc:date>
    </item>
  </channel>
</rss>