<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ghost effect on Custom LCD in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174456#M12050</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For ghost effect: try reducing refresh rate to 30Hz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For "&lt;SPAN class="Apple-style-span"&gt;all segmets appears&lt;SPAN class="Apple-style-span"&gt;": try reducing contrast and use lowest bias mode possible, for example&amp;nbsp;1/3 bias mode.&amp;nbsp;1/2 bias mode is bad at contast ratio.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Apr 2009 23:29:51 GMT</pubDate>
    <dc:creator>BasePointer</dc:creator>
    <dc:date>2009-04-28T23:29:51Z</dc:date>
    <item>
      <title>Ghost effect on Custom LCD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174455#M12049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on a LCD but there is a ghost effect on passive segments. on the other hand when i change viewing angle all segmets appears.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IC is LL64&lt;/P&gt;&lt;P&gt;lcd frequency is 64Hz also lcd capacitance is 35800pF.&lt;/P&gt;&lt;P&gt;This values are so far away that LL16 support but i wanna know ghost effect causes from which conflict?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2009 20:13:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174455#M12049</guid>
      <dc:creator>longliveboy</dc:creator>
      <dc:date>2009-04-22T20:13:41Z</dc:date>
    </item>
    <item>
      <title>Re: Ghost effect on Custom LCD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174456#M12050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For ghost effect: try reducing refresh rate to 30Hz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For "&lt;SPAN class="Apple-style-span"&gt;all segmets appears&lt;SPAN class="Apple-style-span"&gt;": try reducing contrast and use lowest bias mode possible, for example&amp;nbsp;1/3 bias mode.&amp;nbsp;1/2 bias mode is bad at contast ratio.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2009 23:29:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174456#M12050</guid>
      <dc:creator>BasePointer</dc:creator>
      <dc:date>2009-04-28T23:29:51Z</dc:date>
    </item>
    <item>
      <title>Re: Ghost effect on Custom LCD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174457#M12051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi BasePointer;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i already try all freaquency ranges but result is same.&lt;/P&gt;&lt;P&gt;bias is fix at 1/3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;do u know is TN lcds are couses this problem.&lt;/P&gt;&lt;P&gt;i know tn's viewing angle is too narrow but cant guess that it is as bad as mine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;already thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2009 14:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174457#M12051</guid>
      <dc:creator>longliveboy</dc:creator>
      <dc:date>2009-04-29T14:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: Ghost effect on Custom LCD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174458#M12052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes also low quality TN glasses can cause this problem. Try contacting your custom LCD&amp;nbsp;manufacturer and ask for LCD parameters. We did many sample requests from the&amp;nbsp;manufacturer in the past to find perfect lcd solution that has TN glass.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also dont forget, multiplexing reduces total required pin count but it reduces contrast ratio too. We are using 4x40 = 160 segments custom LCD and TN glass without problem. (no ghost effect, wide range viewing angle) We need totally 44 pins. We could also choose 8x20 (28 pins) = 160 segments LCD but, it would have&amp;nbsp;worse&amp;nbsp;contrast ratio.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't have price, industrial temperature range and life time problems, you can choose HTN or STN glass types.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BP.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2009 14:39:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Ghost-effect-on-Custom-LCD/m-p/174458#M12052</guid>
      <dc:creator>BasePointer</dc:creator>
      <dc:date>2009-04-29T14:39:48Z</dc:date>
    </item>
  </channel>
</rss>