<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MC9S08LC60 VREFH and VREFL</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LC60-VREFH-and-VREFL/m-p/174053#M11951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Well, it makes sense....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you bigmac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Jan 2011 02:48:13 GMT</pubDate>
    <dc:creator>rdazcal</dc:creator>
    <dc:date>2011-01-07T02:48:13Z</dc:date>
    <item>
      <title>MC9S08LC60 VREFH and VREFL</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LC60-VREFH-and-VREFL/m-p/174051#M11949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using a MC9S08LC60 MCU and I have VREFH and VREFL pins available externally in the micro-controller.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to connect this pins to different values than VDD and VSS, but I read the following instruction in the data-sheet:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"When available on a separate pin, VREFL must be connected to the same&amp;nbsp;voltage potential as VSSAD."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why is that? Why would it be available externally and not be connected internally in the MCU if the user has no control over it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And why VREFH can't be lower than 1.8V?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jan 2011 21:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LC60-VREFH-and-VREFL/m-p/174051#M11949</guid>
      <dc:creator>rdazcal</dc:creator>
      <dc:date>2011-01-06T21:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08LC60 VREFH and VREFL</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LC60-VREFH-and-VREFL/m-p/174052#M11950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Having the VrefH and VrefL pins externally accessible would permit additional noise filtering to be applied - potentially very useful for 12-bit resolution mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The lower limit on VrefH is similar to the lower limit of Vdd.&amp;nbsp; I presume that, for an even&amp;nbsp;lower VrefH level, the ADC accuracy would deteriorate to an unspecified level.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jan 2011 01:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LC60-VREFH-and-VREFL/m-p/174052#M11950</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-01-07T01:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08LC60 VREFH and VREFL</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LC60-VREFH-and-VREFL/m-p/174053#M11951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Well, it makes sense....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you bigmac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jan 2011 02:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LC60-VREFH-and-VREFL/m-p/174053#M11951</guid>
      <dc:creator>rdazcal</dc:creator>
      <dc:date>2011-01-07T02:48:13Z</dc:date>
    </item>
  </channel>
</rss>