<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173447#M11857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi psy,&lt;BR /&gt;Well you can use the :smileyminus: pin from J103 and TP104 on the back is 5V. There is no easy way!&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 06 Jan 2008 19:11:10 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2008-01-06T19:11:10Z</dc:date>
    <item>
      <title>Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173440#M11850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I have to built up a&amp;nbsp;wireless sensor network by using the 13192SARD boards and the SHT11 humidity sensors.I have a problem in the configuration of the&amp;nbsp;I/O ports of this board and the sensor pins.May&amp;nbsp;anyone&amp;nbsp;experience about it and&amp;nbsp; tell me about the solution&amp;nbsp;?Thanks in advance....&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Dec 2007 12:51:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173440#M11850</guid>
      <dc:creator>psy</dc:creator>
      <dc:date>2007-12-17T12:51:06Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173441#M11851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello, and welcome to the forum.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;The interface requrements&amp;nbsp;for the SHT11 humidity sensor have previously been discussed on this forum.&amp;nbsp; The following thread also provides a link to an earlier thread&amp;nbsp;containing&amp;nbsp;additional information -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=4381" target="_blank"&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/A&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=4381" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=4381&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;The sample code provided by Sensirion will need some adaption to suit the I/O of the Freescale device.&amp;nbsp; Another issue might be the avoidance of floating point calculations, tor the calculation of temperature and humidity.&amp;nbsp; Both these issues were discussed.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2007 01:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173441#M11851</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-12-18T01:19:42Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173442#M11852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks.And for the hardware configuration,if i want to use the PTB 0 and PTB 1,so i have to connect the DATA pin of the sensor to PTB 0 and SCK pin to PTB 1...It is true ??&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2007 22:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173442#M11852</guid>
      <dc:creator>psy</dc:creator>
      <dc:date>2007-12-18T22:40:34Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173443#M11853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;You are correct.&amp;nbsp; However, as explained in a previous thread, the control of the DATA line will need to differ from the sample code, for&amp;nbsp;the HCS08&amp;nbsp;MCU to be compatible with SHT11 requirements - the DATA signal must never be &lt;U&gt;driven&lt;/U&gt; high.&amp;nbsp; This is achieved by controlling the DDR bit, rather than the port register bit.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;For example,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Initialise&amp;nbsp;DATA and CLOCK lines&amp;nbsp;with -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;PTBD_PTBD0 = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* This setting&amp;nbsp;not altered */&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;PTBDD_PTBDD1 = 1;&amp;nbsp; /* CLOCK line is output */&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Set DATA line low -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;PTBDD_PTBDD0 = 1;&amp;nbsp; /* Set pin for output */&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Set DATA line high -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;PTBDD_PTBDD0 = 0;&amp;nbsp; /* Set pin for input/high-Z */&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Set CLOCK line low -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;PTBD_PTBD1 = 0;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Set CLOCK line high -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;PTBD_PTBD1 = 1;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2007 08:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173443#M11853</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-12-19T08:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173444#M11854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;For the hardware configuration,if the sensor need 3V of VDD to operate,hw i can get the 3V of VDD from the 13192SARD board?Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Dec 2007 11:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173444#M11854</guid>
      <dc:creator>psy</dc:creator>
      <dc:date>2007-12-28T11:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173445#M11855</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi psy,&lt;BR /&gt;&lt;BR /&gt;3 volts is available at J103.&lt;BR /&gt;It is marked J103 and 3V and + -.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2008 05:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173445#M11855</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-01-02T05:20:36Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173446#M11856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;If the sensor need 5V of VDD to operate,hw i can get the 5V of VDD from the 13192SARD board?Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Jan 2008 01:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173446#M11856</guid>
      <dc:creator>psy</dc:creator>
      <dc:date>2008-01-05T01:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173447#M11857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi psy,&lt;BR /&gt;Well you can use the :smileyminus: pin from J103 and TP104 on the back is 5V. There is no easy way!&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Jan 2008 19:11:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173447#M11857</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-01-06T19:11:10Z</dc:date>
    </item>
    <item>
      <title>Re: Configuration problem by using 13192SARD boards and the SHT11 humidity</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173448#M11858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;If you wish to operate the SHT11 sensor from Vdd = 5 volt, keep in mind that you will require the complication of additional buffering between the MCU and the sensor&amp;nbsp;- a direct connection would&amp;nbsp;unlikely be feasible.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;For reliable operation, the minimum logic high input to the sensor needs to&amp;nbsp;be greater than&amp;nbsp;4.0 volt, well above the output level provided by the MCU.&amp;nbsp; To prevent damage to the MCU, the pull-up resistor on the data line would need to be sourced from the MCU Vdd.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;There has been&amp;nbsp;discussion of voltage comptibility issues in the following recent thread -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=8640" target="_blank"&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/A&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=8640" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=8640&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Since the data line interface for the sensor requires an "open drain" configuration, the interface method will need to accommodate this requirement.&amp;nbsp; Obvioulsy, it would be much simpler if the sensor Vdd is the same as that for the MCU.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2008 00:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Configuration-problem-by-using-13192SARD-boards-and-the-SHT11/m-p/173448#M11858</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-01-07T00:18:01Z</dc:date>
    </item>
  </channel>
</rss>