<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 HCS08 stop/wait problems</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-stop-wait-problems/m-p/173238#M11800</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Need to talk with someone who is very good with the STOP2 and WAIT functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have code that works, converted it to use WAIT, code broke, I can not determine how to use debugger when using WAIT.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So, of course, removed WAIT from the code and it started working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We are running on batteries so the WAIT function would be better than our current code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Feb 2010 22:16:25 GMT</pubDate>
    <dc:creator>oldone1</dc:creator>
    <dc:date>2010-02-04T22:16:25Z</dc:date>
    <item>
      <title>HCS08 stop/wait problems</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-stop-wait-problems/m-p/173238#M11800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Need to talk with someone who is very good with the STOP2 and WAIT functions.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have code that works, converted it to use WAIT, code broke, I can not determine how to use debugger when using WAIT.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So, of course, removed WAIT from the code and it started working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We are running on batteries so the WAIT function would be better than our current code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2010 22:16:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-stop-wait-problems/m-p/173238#M11800</guid>
      <dc:creator>oldone1</dc:creator>
      <dc:date>2010-02-04T22:16:25Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 stop/wait problems</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-stop-wait-problems/m-p/173239#M11801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;Hi,&amp;nbsp;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;oldone1 wrote:&lt;BR /&gt;&amp;gt;Need to talk with someone who is very good with the STOP2 and WAIT functions.&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&amp;gt;Have code that works, converted it to use WAIT, code broke, I can not determine how &amp;gt;to use debugger when using WAIT.&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;You can't. Or, to be more precise, you can use only a subset of the commands of the debugger (you can't step through code, bu you can see what's in ram, for example). &amp;nbsp;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&amp;gt;So, of course, removed WAIT from the code and it started working.&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&amp;gt;We are running on batteries so the WAIT function would be better than our current code.&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;If going on batteries, the stops are better.&amp;nbsp;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;To solve your problem, try to put toghether a minimal source code that has the problem and post it here (or attach the complete project). Without more information is difficult to help you.&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;Bye Jack&amp;nbsp;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2010 23:41:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-stop-wait-problems/m-p/173239#M11801</guid>
      <dc:creator>jag</dc:creator>
      <dc:date>2010-02-08T23:41:45Z</dc:date>
    </item>
  </channel>
</rss>