<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Entering Run Mode in QG8?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Entering-Run-Mode-in-QG8/m-p/173237#M11799</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Peg,&lt;BR /&gt;Thank you so much for your clarification, am greatly in debt to you. I am going to be using the pin to control the Latch Enable pin so I think it should work ok not grounding the BKGD/MS pin except after POR the latch will be temporarily selected but there isn't any data on the ports, will have to wire it up and see how it turns out.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;Thanks again!&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 16 Dec 2007 23:56:56 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2007-12-16T23:56:56Z</dc:date>
    <item>
      <title>Entering Run Mode in QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Entering-Run-Mode-in-QG8/m-p/173235#M11797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi guys,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I was wondering if anyone know of an easiest way to enter the run mode upon Power-on reset (POR)? It seems that I would need a timer switch debounce circuit to keep the BKGD/MS pin high when power on and then debounce the switch in order to make use of the pin for output.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Would be greatly appreciated if someone put me on the right track.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Dec 2007 23:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Entering-Run-Mode-in-QG8/m-p/173235#M11797</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2007-12-15T23:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: Entering Run Mode in QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Entering-Run-Mode-in-QG8/m-p/173236#M11798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello and welcome, Learner,&lt;BR /&gt;&lt;BR /&gt;You just need to make sure nothing pulls this line low right at power up. If you are using this pin for an output, you don't really need a timer as the code will not change the mode into output until the device is already in run mode.&lt;BR /&gt;So if you are going to put some circuitry on this pin, like a simple base resistor and NPN transistor this will probably cause (or possibly cause) entry into background mode. In this case you will need some additional circuitry in between like a buffer gate or a PNP transistor that then drives the NPN.&lt;BR /&gt;You don't need to actively drive this pin high, just don't bias it low!&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Dec 2007 06:05:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Entering-Run-Mode-in-QG8/m-p/173236#M11798</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-12-16T06:05:31Z</dc:date>
    </item>
    <item>
      <title>Re: Entering Run Mode in QG8?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Entering-Run-Mode-in-QG8/m-p/173237#M11799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Peg,&lt;BR /&gt;Thank you so much for your clarification, am greatly in debt to you. I am going to be using the pin to control the Latch Enable pin so I think it should work ok not grounding the BKGD/MS pin except after POR the latch will be temporarily selected but there isn't any data on the ports, will have to wire it up and see how it turns out.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;Thanks again!&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Dec 2007 23:56:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Entering-Run-Mode-in-QG8/m-p/173237#M11799</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2007-12-16T23:56:56Z</dc:date>
    </item>
  </channel>
</rss>