<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: BeeStack Address Map table and Binding table, MC1322x in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172812#M11775</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this thread is actually about another topic, however: There exists an own occupancy sensing cluster, why not use this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;greets&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Feb 2010 18:50:37 GMT</pubDate>
    <dc:creator>sverige</dc:creator>
    <dc:date>2010-02-18T18:50:37Z</dc:date>
    <item>
      <title>BeeStack Address Map table and Binding table, MC1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172808#M11771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a network node as coordinator, a sensor node as router and another sensor node as end device. The coordinator form the network and the router and end device join to that network. Then I make a binding between the router and the end device. In that moment there are tables with the mac address of&amp;nbsp; all the devices that are in the networik so I would like to save all this configuration in the non volatil memory in the coordinator but I dont know how can I do that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Where is the mac address table and the binding table? All that information is accesible from coordinator if the network is formed,doesn't it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Teresa Seco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Feb 2010 19:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172808#M11771</guid>
      <dc:creator>tseco</dc:creator>
      <dc:date>2010-02-03T19:30:48Z</dc:date>
    </item>
    <item>
      <title>Re: BeeStack Address Map table and Binding table, MC1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172809#M11772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you are looking for the address map which links IEEE Addresses to short adresses gaApsAddressMap&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and the Binding Table.&lt;/P&gt;&lt;P&gt;gaApsBindingTable&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Both tables are automatically stored to NVM, so you should not have to modify this. The NVM Dataset it uses is: NvDataSetTable&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Binding table gets set up when you configure binding (e.g. by pressing the binding key on the nodes), not already after the ZC formed the network.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;hope i could help,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;greets,&lt;/P&gt;&lt;P&gt;Franz&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by sverige on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2010-02-12&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;05:40 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Feb 2010 00:38:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172809#M11772</guid>
      <dc:creator>sverige</dc:creator>
      <dc:date>2010-02-13T00:38:13Z</dc:date>
    </item>
    <item>
      <title>Re: BeeStack Address Map table and Binding table, MC1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172810#M11773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much for your answer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have another question. In what moment is saved in the NVM tha binding table? Where is that table, in the coordinator?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My network has a coordinator, a end device and a router. I bind the end device with the router but when I ask to the coordinator about the binding table, there is nothing in that table.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use this call for the binding table in the coordinator:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;apsBindingTable_t bindingTable[gMaximumApsBindingTableEntries_c];&lt;BR /&gt;&amp;nbsp; uint8_t index = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;for (index = 0;index&amp;lt;gMaximumApsBindingTableEntries_c;index++)&lt;BR /&gt;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FLib_MemCpy(&amp;amp;bindingTable[index],(void*)(ApsmeGetRequest_gApsBindingTable_c(index)), sizeof(bindingTable[index]));&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Any suggestions?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Teresa&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Feb 2010 20:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172810#M11773</guid>
      <dc:creator>tseco</dc:creator>
      <dc:date>2010-02-17T20:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: BeeStack Address Map table and Binding table, MC1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172811#M11774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I read in one of your post that you made your own occupancy sensor device. I thought to use one of the devices available in the Freescale ZCL for this purpose, but I do not know which one is the most suitable, perhaps temperature sensor?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Could you give some indication about how to develop my own occupancy sensor device? If I add this endpoint to my end device, I need another input endpoint for the binding, so I must to develop another new device, am I right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any helo would be very useful for me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Teresa Seco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2010 17:50:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172811#M11774</guid>
      <dc:creator>tseco</dc:creator>
      <dc:date>2010-02-18T17:50:31Z</dc:date>
    </item>
    <item>
      <title>Re: BeeStack Address Map table and Binding table, MC1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172812#M11775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this thread is actually about another topic, however: There exists an own occupancy sensing cluster, why not use this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;greets&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2010 18:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172812#M11775</guid>
      <dc:creator>sverige</dc:creator>
      <dc:date>2010-02-18T18:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: BeeStack Address Map table and Binding table, MC1322x</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172813#M11776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hI,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; In the Freescale ZCL reference manual (ZCLRM) there is a lis with the clusters and their attributes supported by the BeeStack ZCL and the occupancy sensor does not appear in this list and when I try to add a endpoint the beekit does not offer the option of occupancy sensor...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Could you give me some indications about the binding table question that I asked before this question?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2010 18:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BeeStack-Address-Map-table-and-Binding-table-MC1322x/m-p/172813#M11776</guid>
      <dc:creator>tseco</dc:creator>
      <dc:date>2010-02-18T18:58:59Z</dc:date>
    </item>
  </channel>
</rss>