<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MCG external crystal for usb - s08JM60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172513#M11749</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear trav,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using WTUSBDM there is an option to use a different clock source for the BDM interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the dialogue that pop ups when connecting try selecting "Force BDM clock source"&amp;nbsp; and try the two alternatives.&amp;nbsp; If you're lucky one should work ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Apr 2009 18:40:43 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2009-04-18T18:40:43Z</dc:date>
    <item>
      <title>MCG external crystal for usb - s08JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172510#M11746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a s08JM60 I am trying to use the usb module on, and one of the requirements is that I have an external clock so I can have a 24Mhz bus clock.&amp;nbsp; I have app note AN3560 which has code for an external 12Mhz crystal, which is what I have.&amp;nbsp; But when I run the MCG_Init() it errors out with an ILLEGAL BP.&amp;nbsp; Once I get this error I can not reconnect to the chip without a reset.&amp;nbsp; I get an unable to execute command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the code from the app note.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;
void MCG_Init(){/* the MCG is set to FEI mode by default, it should be change to FBE mode at first */MCGC2 = 0x36;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Select high frequency, high gain, Oscillator requested*/while(!(MCGSC &amp;amp; 0x02));&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Wait for the stable of Oscillator */MCGC1 = 0x9B;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*External clock is selected, RDIV = 0b011 (to get 1.5MHz)*/while((MCGSC &amp;amp; 0x1C) != 0x08);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Check whether the external reference clock is selected */&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Switch to PBE mode from FBE*/MCGC3 = 0x48;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Enable PLL, VDIV = 0b1000, multiply by 32*/while ((MCGSC &amp;amp; 0x48) != 0x48);&amp;nbsp;&amp;nbsp; /*Wait for the PLL to be locked */&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Switch to PEE mode from PBE mode*/MCGC1 &amp;amp;= 0x3F;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*PLL output is selected*/while((MCGSC &amp;amp; 0x6C) != 0x6C);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Wait for the PLL output becoming the system clock source */return;}&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The error starts at either the MCGC1 &amp;amp;= 0x3F;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;or&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;while((MCGSC &amp;amp; 0x6C) != 0x6C);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could wrong value capacitors cause this?&amp;nbsp; It does kick start crystal as I can see a 12Mhz signal on the scope.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Travis&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Added p/n to subject.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by NLFSJ on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-04-16&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;09:17 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172510#M11746</guid>
      <dc:creator>trav</dc:creator>
      <dc:date>2020-10-29T09:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: MCG external crystal for usb - s08JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172511#M11747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear trav,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What BDM are you using?&amp;nbsp; Some have a limited range of speeds over which they will operate.&amp;nbsp; You will get similar symptoms if this is the case.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using OSBDM check the communication speed in the debugger after you lose communication. (under status?)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For reference: My code to configure the MCG is given below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="1"&gt;//==========================================&lt;BR /&gt;// Sets up the clock for USB operation&lt;BR /&gt;// MGCOUT = 48MHz, BUS_CLOCK = 24MHz, (PEE mode)&lt;BR /&gt;//&lt;BR /&gt;// Assumes 12 MHz external crystal&lt;BR /&gt;//&lt;BR /&gt;// Modes: FEI (FLL engaged internal) -&amp;gt;&lt;BR /&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FBE (FLL bypassed external) -&amp;gt;&lt;BR /&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PBE (PLL bypassed external) -&amp;gt;&lt;BR /&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PEE (PLL engaged external)&lt;BR /&gt;//&lt;BR /&gt;// Refer 12.5.2.1 of MC9S08JM60 Reference&lt;BR /&gt;//&lt;BR /&gt;static void init_clock(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // Out of reset MCG is in FEI mode&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 1. Switch from FEI (FLL engaged internal) to FBE (FLL bypassed external)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 1 a) Set up crystal&lt;BR /&gt;&amp;nbsp;&amp;nbsp; MCGC2 =&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // BDIV = 0, divide by 1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCGC2_HGO_MASK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // oscillator in high gain mode&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | MCGC2_EREFS_MASK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // because crystal is being used&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | MCGC2_RANGE_MASK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // 12 MHz is in high freq range&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | MCGC2_ERCLKEN_MASK;&amp;nbsp; // activate external reference clock&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 1 b) Wait for crystal to start up&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; while (MCGSC_OSCINIT == 0) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 1 c) Select clock mode&lt;BR /&gt;&amp;nbsp;&amp;nbsp; MCGC1 =&amp;nbsp;&amp;nbsp; (2&amp;lt;&amp;lt;6)&amp;nbsp;&amp;nbsp; // CLKS = 10 -&amp;gt; External reference clock&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | (3&amp;lt;&amp;lt;3);&amp;nbsp; // RDIV = 3&amp;nbsp; -&amp;gt; 12MHz/8=1.5 MHz&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 1 d) Wait for mode change&lt;BR /&gt;&amp;nbsp;&amp;nbsp; while (MCGSC_IREFST != 0) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 1 e) Wait for MCGOUT indicating that the external reference to be fed to MCGOUT&lt;BR /&gt;&amp;nbsp;&amp;nbsp; while (MCGSC_CLKST != 2) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 2. Switch FBE (FLL bypassed external) to PBE (PLL Bypassed External) mode&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 2 b) Set RDIV for correct range&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 2 c) Enable the PLL &amp;amp; set VDIV value&lt;BR /&gt;&amp;nbsp;&amp;nbsp; MCGC3 = MCGC3_PLLS_MASK&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | (8&amp;lt;&amp;lt;0);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // VDIV=6 -&amp;gt; multiply by 32 -&amp;gt; 1.5MHz * 32 = 48MHz */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 2 e) Wait until PLLS clock source changes to the PLL&lt;BR /&gt;&amp;nbsp;&amp;nbsp; while(MCGSC_PLLST != 1) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 2 f)&amp;nbsp; Wait for PLL to acquired lock&lt;BR /&gt;&amp;nbsp;&amp;nbsp; while(MCGSC_LOCK != 1) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 3. PBE mode transitions into PEE mode:&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 3 a) Set RDIV for correct range and select PLL.FLL clock&lt;BR /&gt;&amp;nbsp;&amp;nbsp; MCGC1 =&amp;nbsp;&amp;nbsp; (0&amp;lt;&amp;lt;6)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // CLKS = 0 -&amp;gt; PLL or FLL output clock&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; | (3&amp;lt;&amp;lt;3);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // RDIV = 3 -&amp;gt; 12MHz/8=1.5 MHz (req. 1 &amp;lt; f &amp;lt; 2)&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // 3 c)&amp;nbsp; Wait for clock stable&lt;BR /&gt;&amp;nbsp;&amp;nbsp; while(MCGSC_CLKST!=3) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; /* Now MCGOUT=48MHz, BUS_CLOCK=24MHz */&amp;nbsp;&lt;BR /&gt;}&lt;/FONT&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by pgo on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-04-18&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;05:29 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by pgo on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-04-18&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;05:29 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Apr 2009 14:23:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172511#M11747</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-04-18T14:23:00Z</dc:date>
    </item>
    <item>
      <title>Re: MCG external crystal for usb - s08JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172512#M11748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using a &lt;SPAN class="smallText"&gt;WTUSBDML which is a witztronic bdm.&amp;nbsp; After reading the specs for it again on thier web page, it does say a limit bus speed of 20Mhz.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="smallText"&gt;The OSBDM status did say 48Mhz, but the BDM status reg right about it reads 0x64(secured?).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question now is what bdm's support speeds that fast.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Travis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Apr 2009 18:22:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172512#M11748</guid>
      <dc:creator>trav</dc:creator>
      <dc:date>2009-04-18T18:22:11Z</dc:date>
    </item>
    <item>
      <title>Re: MCG external crystal for usb - s08JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172513#M11749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear trav,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are using WTUSBDM there is an option to use a different clock source for the BDM interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the dialogue that pop ups when connecting try selecting "Force BDM clock source"&amp;nbsp; and try the two alternatives.&amp;nbsp; If you're lucky one should work ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Apr 2009 18:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172513#M11749</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-04-18T18:40:43Z</dc:date>
    </item>
    <item>
      <title>Re: MCG external crystal for usb - s08JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172514#M11750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes this worked!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had to install the opensourcebdm.dll file, because I was not seeing the menu you were talking about.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Apr 2009 06:09:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCG-external-crystal-for-usb-s08JM60/m-p/172514#M11750</guid>
      <dc:creator>trav</dc:creator>
      <dc:date>2009-04-19T06:09:52Z</dc:date>
    </item>
  </channel>
</rss>