<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Program will not run standalone on QE8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172215#M11705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I wrote a program and downloaded it into the DEMOQE demo board and QE8&amp;nbsp;uC with the CodeWarrior debugger and it runs just fine. It does everything I asked it to do.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I can download the program and run it&amp;nbsp;and it runs great but if I shutdown CW and I power cycle the DEMOQE board the program won't run on it's own. It acts like it's dependent on CW.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Does anyone have any ideas&amp;nbsp;as to why a program won't run on it's own once it is downloaded into the uC?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Rodo&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jul 2008 11:17:45 GMT</pubDate>
    <dc:creator>Rodo55</dc:creator>
    <dc:date>2008-07-11T11:17:45Z</dc:date>
    <item>
      <title>Program will not run standalone on QE8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172215#M11705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I wrote a program and downloaded it into the DEMOQE demo board and QE8&amp;nbsp;uC with the CodeWarrior debugger and it runs just fine. It does everything I asked it to do.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I can download the program and run it&amp;nbsp;and it runs great but if I shutdown CW and I power cycle the DEMOQE board the program won't run on it's own. It acts like it's dependent on CW.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Does anyone have any ideas&amp;nbsp;as to why a program won't run on it's own once it is downloaded into the uC?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Rodo&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2008 11:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172215#M11705</guid>
      <dc:creator>Rodo55</dc:creator>
      <dc:date>2008-07-11T11:17:45Z</dc:date>
    </item>
    <item>
      <title>Re: Program will not run standalone on QE8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172216#M11706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Please do not post the same problem to multiple forums, at least not with mentioning that so that duplicated answers are avoided.&lt;BR /&gt;To check:&lt;BR /&gt;- do you handle or disable the COP?&lt;BR /&gt;- is the reset vector set?&lt;BR /&gt;- check write once registers, with the debugger they can be written multiple times but not in normal modes.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2008 12:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172216#M11706</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2008-07-11T12:01:23Z</dc:date>
    </item>
    <item>
      <title>Re: Program will not run standalone on QE8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172217#M11707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Rodo55,&lt;BR /&gt;&lt;BR /&gt;I agree with CompilerGuru: this is a typical case of not servicing the watchdog (COP).&lt;BR /&gt;&lt;BR /&gt;While in debug mode the COP is automatically disabled. If you are not disabling the COP in the SOPT1 register, chances are that the COP is timing out and resetting the CPU.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jul 2008 04:20:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172217#M11707</guid>
      <dc:creator>fabio</dc:creator>
      <dc:date>2008-07-17T04:20:52Z</dc:date>
    </item>
    <item>
      <title>Re: Program will not run standalone on QE8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172218#M11708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Fabio,&lt;BR /&gt;&lt;BR /&gt;See the &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&amp;amp;message.id=5898" target="_blank"&gt;other version of this thread&lt;/A&gt; and see if you still agree.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jul 2008 04:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-will-not-run-standalone-on-QE8/m-p/172218#M11708</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-07-17T04:31:20Z</dc:date>
    </item>
  </channel>
</rss>