<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: USB connectivity in the S08JM60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-connectivity-in-the-S08JM60/m-p/172144#M11704</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sound like the PC class driver hangs, rather than a problem of USB connection.&lt;BR /&gt;1) What is the OS, Windows?&lt;BR /&gt;2) What is the USB class?&lt;BR /&gt;&lt;BR /&gt;&amp;gt; but the source of trouble in USB communication is the driver in the host PC side that needs a reboot of the host PC.&lt;BR /&gt;&lt;BR /&gt;Soft-detach / attach on the device will work to release the PC class driver from hang.&lt;BR /&gt;&lt;BR /&gt;Tsuneo﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Oct 2011 21:23:38 GMT</pubDate>
    <dc:creator>Tsuneo</dc:creator>
    <dc:date>2011-10-06T21:23:38Z</dc:date>
    <item>
      <title>USB connectivity in the S08JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-connectivity-in-the-S08JM60/m-p/172143#M11703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;BR /&gt;&lt;BR /&gt;I am working with the JM32 microcontroller and trying to detect&lt;BR /&gt;the USB connectivity between the micro and the host PC.&lt;BR /&gt;Can i check the connectivity in the USB_ISR() : Interrupt 7.&lt;BR /&gt;&lt;BR /&gt;This will help me reset the host PC when there is no USB communication.&lt;BR /&gt;USB cable is attached correctly, but the source of trouble in USB communication&lt;BR /&gt;is the driver in the host PC side that needs a reboot of the host PC.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Oct 2011 20:54:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-connectivity-in-the-S08JM60/m-p/172143#M11703</guid>
      <dc:creator>OualBel</dc:creator>
      <dc:date>2011-10-05T20:54:21Z</dc:date>
    </item>
    <item>
      <title>Re: USB connectivity in the S08JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-connectivity-in-the-S08JM60/m-p/172144#M11704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sound like the PC class driver hangs, rather than a problem of USB connection.&lt;BR /&gt;1) What is the OS, Windows?&lt;BR /&gt;2) What is the USB class?&lt;BR /&gt;&lt;BR /&gt;&amp;gt; but the source of trouble in USB communication is the driver in the host PC side that needs a reboot of the host PC.&lt;BR /&gt;&lt;BR /&gt;Soft-detach / attach on the device will work to release the PC class driver from hang.&lt;BR /&gt;&lt;BR /&gt;Tsuneo﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2011 21:23:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-connectivity-in-the-S08JM60/m-p/172144#M11704</guid>
      <dc:creator>Tsuneo</dc:creator>
      <dc:date>2011-10-06T21:23:38Z</dc:date>
    </item>
  </channel>
</rss>