<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RE: HC908QT4 Internal osc. in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RE-HC908QT4-Internal-osc/m-p/126642#M1167</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi wf.lee&lt;BR /&gt;Since the bus clock is one fourth of f osc -&amp;gt; this is correct! The internal osc runs at 12.8MHz (nominal, +/-25%) so maximum bus clock frequency will bee 4MHz (means f osz = 16MHz). For a adjusted osz. frquency you have to programm the OSCTRIM register with the right value.&lt;BR /&gt;&lt;BR /&gt;Saluti joerg&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2006 04:10:54 GMT</pubDate>
    <dc:creator>joerg</dc:creator>
    <dc:date>2006-02-22T04:10:54Z</dc:date>
    <item>
      <title>RE: HC908QT4 Internal osc.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RE-HC908QT4-Internal-osc/m-p/126641#M1166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm using HC908QT4 and internal osc. I've set the OSCOPT1:0 to 00 in CONFIG2 but the OSC2 on PTA4 (OSC2EN=1) shown it's only ~3.9MHz not 12.8MHz as stated in the datasheet.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any suggestion what goes wrong? Thx!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Feb 2006 23:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RE-HC908QT4-Internal-osc/m-p/126641#M1166</guid>
      <dc:creator>wf_lee</dc:creator>
      <dc:date>2006-02-20T23:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: RE: HC908QT4 Internal osc.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RE-HC908QT4-Internal-osc/m-p/126642#M1167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi wf.lee&lt;BR /&gt;Since the bus clock is one fourth of f osc -&amp;gt; this is correct! The internal osc runs at 12.8MHz (nominal, +/-25%) so maximum bus clock frequency will bee 4MHz (means f osz = 16MHz). For a adjusted osz. frquency you have to programm the OSCTRIM register with the right value.&lt;BR /&gt;&lt;BR /&gt;Saluti joerg&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2006 04:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RE-HC908QT4-Internal-osc/m-p/126642#M1167</guid>
      <dc:creator>joerg</dc:creator>
      <dc:date>2006-02-22T04:10:54Z</dc:date>
    </item>
  </channel>
</rss>