<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: PLEASE HELP ME: background mode Problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PLEASE-HELP-ME-background-mode-Problem/m-p/171731#M11630</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for reply&lt;/P&gt;&lt;P&gt;I solved the problem. It was due to disconnection of the board ground and programmer ground pin in flat cable. So when I used USB supply, the two groud was connected through the computer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Apr 2009 14:49:29 GMT</pubDate>
    <dc:creator>bitasobhani</dc:creator>
    <dc:date>2009-04-15T14:49:29Z</dc:date>
    <item>
      <title>PLEASE HELP ME: background mode Problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PLEASE-HELP-ME-background-mode-Problem/m-p/171729#M11628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;I cannot program 1321x SRB board by a BDM programmer when I use switching power supply (yellow led on programmer is OFF). But when I use USB supply it can be programmed (yellow led on programmer is ON). I have the same problem when programming 13192 SARD board whith switching power supply. Unfortunately the board has no USB connector. So I cannot program the board at all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I measured switching power supply voltage with voltmeter. It is 9.15volt.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2009 14:33:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PLEASE-HELP-ME-background-mode-Problem/m-p/171729#M11628</guid>
      <dc:creator>bitasobhani</dc:creator>
      <dc:date>2009-04-14T14:33:03Z</dc:date>
    </item>
    <item>
      <title>Re: PLEASE HELP ME: background mode Problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PLEASE-HELP-ME-background-mode-Problem/m-p/171730#M11629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the SARD board work with a 9V battery?&lt;/P&gt;&lt;P&gt;Does the green power LED on the SARD come on with the external power supply like it does with the battery?&lt;/P&gt;&lt;P&gt;You do realise the power switch works opposite when using external power supply.&lt;/P&gt;&lt;P&gt;Can you measure 3 volts on the 2 pins behind the serial socket? (marked 3V and + -)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2009 04:49:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PLEASE-HELP-ME-background-mode-Problem/m-p/171730#M11629</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-04-15T04:49:35Z</dc:date>
    </item>
    <item>
      <title>Re: PLEASE HELP ME: background mode Problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PLEASE-HELP-ME-background-mode-Problem/m-p/171731#M11630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for reply&lt;/P&gt;&lt;P&gt;I solved the problem. It was due to disconnection of the board ground and programmer ground pin in flat cable. So when I used USB supply, the two groud was connected through the computer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2009 14:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PLEASE-HELP-ME-background-mode-Problem/m-p/171731#M11630</guid>
      <dc:creator>bitasobhani</dc:creator>
      <dc:date>2009-04-15T14:49:29Z</dc:date>
    </item>
  </channel>
</rss>