<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flashing blank MC13213 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171613#M11603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;DeedsBee,&lt;BR /&gt;&lt;BR /&gt;Once you solder the chip to the board, please make sure that VDD, GND, RESET and BKND connections to the 6 pin BDM header are solid. Also, the BKND and RESET pins should be pulled up to VDD with a 4.7-10k resistor.&lt;BR /&gt;&lt;BR /&gt;Once you provide power to the chip, you should see a yellow LED on a USB Multilink light up.&lt;BR /&gt;&lt;BR /&gt;What is the voltage on the external power supply that you are using to power up your setup?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zahar&lt;BR /&gt;P&amp;amp;E&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jul 2008 21:02:26 GMT</pubDate>
    <dc:creator>Zahar</dc:creator>
    <dc:date>2008-07-24T21:02:26Z</dc:date>
    <item>
      <title>Flashing blank MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171610#M11600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Ok guys, after hours and hours trying to flash my module (thousand of "power cycling" in CodeWarrior using P&amp;amp;E Multilink) I still just ca't get it working. It doesn't enter in Background Debug Mode. I tried power off and power on while holding BKGD pin low, but no success... I read a lot of posts here about flashing blank devices and I see that is not just me with this problem. I have the following voltage in the pins:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;3V in VBATT and VDDINT (the power supply is good, no significant noise);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;0V in VDDVCO (?) (I think it's because MCU keeps executing COP reset (blank device), right?);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;~0.3V in VDDA, VDDLO1 and VDDLO2&amp;nbsp;(?) (again, is COP reset the cause?);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;~2V in reset pin (?) (this is really strange, but again I'm blaming COP reset &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt; );&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;3V in BKGD (I tried the power cycle holding BKGD low);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Well, anyone please help me! I'm working in solder issues too, but it appears that every connection is fine. Thanks in advance!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;DedsBee&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 21:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171610#M11600</guid>
      <dc:creator>DedsBee</dc:creator>
      <dc:date>2008-07-09T21:17:20Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing blank MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171611#M11601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi DedsBee,&lt;BR /&gt;&lt;BR /&gt;Firstly, I presume you have seen &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=OSBDM08&amp;amp;message.id=136" target="_blank"&gt;this thread&lt;/A&gt;.&lt;BR /&gt;The notes about GB should apply to your device.&lt;BR /&gt;If you have a blank device and pull BKGD low for more than a COP period it will enter Background mode.&lt;BR /&gt;I would be putting a scope on your reset pin to see if it sheds any light on what is happening.&lt;BR /&gt;2 volts is wrong, the COP pulses are a very low duty and any device would still read very close to full volts.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2008 05:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171611#M11601</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-07-10T05:52:37Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing blank MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171612#M11602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Peg!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; Yeah, I think you are right about 2V in my reset pin. It´s really wrong. I checked in a scope and there is no "pulse" or something like that. It´s steady in ~1.5V.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; And about the voltages in VDDA, VDDD and VDDVCO? Do you think it´s wrong too? Even with COP resets the voltages should be 1.8V?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; Well, I gived up about flashing. Now I´m focus in solder issues. Looking closer, it appears that the chip is "floating" over some pins. Oh my, that chip is really hard to work with manual solder.. I should receive 2 more boards next week, so the chances to get at least 1 working grows up.. &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt; Thank you Peg, I will post any news.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;DedsBee&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2008 07:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171612#M11602</guid>
      <dc:creator>DedsBee</dc:creator>
      <dc:date>2008-07-10T07:21:19Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing blank MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171613#M11603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;DeedsBee,&lt;BR /&gt;&lt;BR /&gt;Once you solder the chip to the board, please make sure that VDD, GND, RESET and BKND connections to the 6 pin BDM header are solid. Also, the BKND and RESET pins should be pulled up to VDD with a 4.7-10k resistor.&lt;BR /&gt;&lt;BR /&gt;Once you provide power to the chip, you should see a yellow LED on a USB Multilink light up.&lt;BR /&gt;&lt;BR /&gt;What is the voltage on the external power supply that you are using to power up your setup?&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zahar&lt;BR /&gt;P&amp;amp;E&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2008 21:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Flashing-blank-MC13213/m-p/171613#M11603</guid>
      <dc:creator>Zahar</dc:creator>
      <dc:date>2008-07-24T21:02:26Z</dc:date>
    </item>
  </channel>
</rss>