<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Hyperterminal and DEMOQE128 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171391#M11550</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi.&lt;BR /&gt;&lt;BR /&gt;Are you using the DB9 attached?&lt;BR /&gt;In this case you need to enable Max3218, you need change jumper J205 and set PTC5 to 1 in order to enable MAX IC.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by erooll on &lt;SPAN class="date_text"&gt;2008-07-08&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:26 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jul 2008 09:21:23 GMT</pubDate>
    <dc:creator>erooll</dc:creator>
    <dc:date>2008-07-09T09:21:23Z</dc:date>
    <item>
      <title>Hyperterminal and DEMOQE128</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171390#M11549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using DEMOQE128 board. I am using SCI to transmit a charachter 'H' and display it on the hyperterminal(XP). But i cannot see anything on the hyperterminal. My baud rate is 9600. I think the busclock is 4MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please help me out.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 06:52:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171390#M11549</guid>
      <dc:creator>shumpi55</dc:creator>
      <dc:date>2008-07-09T06:52:28Z</dc:date>
    </item>
    <item>
      <title>Re: Hyperterminal and DEMOQE128</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171391#M11550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi.&lt;BR /&gt;&lt;BR /&gt;Are you using the DB9 attached?&lt;BR /&gt;In this case you need to enable Max3218, you need change jumper J205 and set PTC5 to 1 in order to enable MAX IC.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by erooll on &lt;SPAN class="date_text"&gt;2008-07-08&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:26 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 09:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171391#M11550</guid>
      <dc:creator>erooll</dc:creator>
      <dc:date>2008-07-09T09:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: Hyperterminal and DEMOQE128</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171392#M11551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have enabled PTC5. There is no jumper J205 in this board. i am using MC9S08QE128 micro-controller. I am using the DB9 attached to the board.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 19:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171392#M11551</guid>
      <dc:creator>shumpi55</dc:creator>
      <dc:date>2008-07-09T19:54:08Z</dc:date>
    </item>
    <item>
      <title>Re: Hyperterminal and DEMOQE128</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171393#M11552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;J8 jumper could be removed at all and R9 pullup will enable MAX3218. J8 can be also set to PTC5 position. Either you drive PTC5 high or leave it in default input mode (R8 pullup will enable MAX3218).&lt;/DIV&gt;&lt;DIV&gt;Did you reconfigure J7 and J8 from USB-TX/RX to MAX-TX/RX? In USB position you can send/receive only via USB and P&amp;amp;E terminal program. Having J7 and J8 in&amp;nbsp;MAX-TX/RX&amp;nbsp;you send/receive only via DB9 connector.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 20:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171393#M11552</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2008-07-09T20:52:40Z</dc:date>
    </item>
    <item>
      <title>Re: Hyperterminal and DEMOQE128</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171394#M11553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;how do I set J7 and J8 in Max Tx/Rx ?&lt;BR /&gt;My program is as follows:&lt;BR /&gt;SCI1C1=0x40;&lt;BR /&gt;SCI1C2=0x08;&lt;BR /&gt;PTCDD_PTCDD5=1;&lt;BR /&gt;PTCD_PTCD=1;&lt;BR /&gt;SCIBDL=0x1A;//baud rate=9600bps and bus freq=4MHz.&lt;BR /&gt;for(;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;{&lt;BR /&gt;while((SCI1S1 &amp;amp; 0x80)==0);&lt;BR /&gt;SCI1D='H';&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 22:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171394#M11553</guid>
      <dc:creator>shumpi55</dc:creator>
      <dc:date>2008-07-09T22:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: Hyperterminal and DEMOQE128</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171395#M11554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;J6, J7 and J8 are jumpers on the DEMOQE, close to RS232 connector. DEMOQE schematic&amp;nbsp;should be on your PC if you installed P&amp;amp;E DemoQE toolkit.&lt;/DIV&gt;&lt;DIV&gt;Your code looks&amp;nbsp;good and should work.&lt;/DIV&gt;&lt;DIV&gt;Also you may save a lot of time using easier than Hyperterminal program, like this free one from Elmicro : &lt;A href="http://elmicro.com/files/occonsole_v30.zip" rel="nofollow" target="_blank"&gt;http://elmicro.com/files/occonsole_v30.zip&lt;/A&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by kef on &lt;SPAN class="date_text"&gt;2008-07-09&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;07:01 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 22:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Hyperterminal-and-DEMOQE128/m-p/171395#M11554</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2008-07-09T22:52:06Z</dc:date>
    </item>
  </channel>
</rss>