<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IGC Trim does match Flashed Trim on reset in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IGC-Trim-does-match-Flashed-Trim-on-reset/m-p/171334#M11535</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the MC9S08GT16, CW 6.3, P+E USB multilink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Debug I can see the IGC trim value in 0x004E matches the FLASH value in 0xFFBE&lt;/P&gt;&lt;P&gt;Resetting the part through the debugger also places the value from Flash into the IGC trim reg (or at least they are the same)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is when the debugger is not attached and I do a power cycle. Fortunately on this particular chip the trim is almost 0 (actually 0x88) so I can communicate via serial port. When I look at register 0x004E it has the default value (0x80) even though the flash has the value 0x88.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the part actually use location 0xFFBE on reset? Spec sheet says it does.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jun 2012 23:13:32 GMT</pubDate>
    <dc:creator>zigbertsschec</dc:creator>
    <dc:date>2012-06-11T23:13:32Z</dc:date>
    <item>
      <title>IGC Trim does match Flashed Trim on reset</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IGC-Trim-does-match-Flashed-Trim-on-reset/m-p/171334#M11535</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the MC9S08GT16, CW 6.3, P+E USB multilink&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In Debug I can see the IGC trim value in 0x004E matches the FLASH value in 0xFFBE&lt;/P&gt;&lt;P&gt;Resetting the part through the debugger also places the value from Flash into the IGC trim reg (or at least they are the same)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is when the debugger is not attached and I do a power cycle. Fortunately on this particular chip the trim is almost 0 (actually 0x88) so I can communicate via serial port. When I look at register 0x004E it has the default value (0x80) even though the flash has the value 0x88.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the part actually use location 0xFFBE on reset? Spec sheet says it does.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jun 2012 23:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IGC-Trim-does-match-Flashed-Trim-on-reset/m-p/171334#M11535</guid>
      <dc:creator>zigbertsschec</dc:creator>
      <dc:date>2012-06-11T23:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: IGC Trim does match Flashed Trim on reset</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/IGC-Trim-does-match-Flashed-Trim-on-reset/m-p/171335#M11536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora, zigbert.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The part DOES NOT use location 0xFFBE on reset!&lt;/P&gt;&lt;P&gt;It is up to your code to copy it across manually.&lt;/P&gt;&lt;P&gt;Perhaps you could indicate to us where the manual says that it does so...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P.S. this question has been nswered many times on the forum. Some searching before posting is correct usage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2012 05:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/IGC-Trim-does-match-Flashed-Trim-on-reset/m-p/171335#M11536</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2012-06-12T05:24:42Z</dc:date>
    </item>
  </channel>
</rss>