<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DEMO9S08QG8_APP Error. in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9S08QG8-APP-Error/m-p/171321#M11532</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Dimy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have not checked, but it is possible that this macro may already be defined within the header file for the QG8 device.&amp;nbsp; If this is the case, you can probably "comment out" the second definition of the macro within the project file.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The demo code may have originally been compiled using an earlier version of CW that did not already contain the macro definition.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jul 2008 10:56:23 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-07-09T10:56:23Z</dc:date>
    <item>
      <title>DEMO9S08QG8_APP Error.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9S08QG8-APP-Error/m-p/171320#M11531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello, a got the source for the DEMO9S08QG8_APP from the forum and I can't compile the file because of an error in codeWarrior: c4402 Redefinition of existing macro 'NVICSTRM'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I didn't made any alteration to the source, so I am not sure what to do.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any help would be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Dimy.&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 00:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9S08QG8-APP-Error/m-p/171320#M11531</guid>
      <dc:creator>Dimy</dc:creator>
      <dc:date>2008-07-09T00:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO9S08QG8_APP Error.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9S08QG8-APP-Error/m-p/171321#M11532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Dimy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have not checked, but it is possible that this macro may already be defined within the header file for the QG8 device.&amp;nbsp; If this is the case, you can probably "comment out" the second definition of the macro within the project file.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The demo code may have originally been compiled using an earlier version of CW that did not already contain the macro definition.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jul 2008 10:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9S08QG8-APP-Error/m-p/171321#M11532</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-07-09T10:56:23Z</dc:date>
    </item>
  </channel>
</rss>