<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピックmc68hc908gp32 bootloader</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170601#M11411</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;is there a way how to force mc68hc908 mcu to enter in the bootloader to change the firmware to new one. really appreciate your kind help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Sep 2011 03:49:01 GMT</pubDate>
    <dc:creator>mc68hc908</dc:creator>
    <dc:date>2011-09-29T03:49:01Z</dc:date>
    <item>
      <title>mc68hc908gp32 bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170601#M11411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;is there a way how to force mc68hc908 mcu to enter in the bootloader to change the firmware to new one. really appreciate your kind help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2011 03:49:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170601#M11411</guid>
      <dc:creator>mc68hc908</dc:creator>
      <dc:date>2011-09-29T03:49:01Z</dc:date>
    </item>
    <item>
      <title>Re: mc68hc908gp32 bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170602#M11412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That would depend on the bootloader you have installed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you mean to enter Monitor mode then it is all spelled out in the &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=HC08G&amp;amp;tab=Documentation_Tab&amp;amp;pspll=1&amp;amp;SelectedAsset=Documentation&amp;amp;ProdMetaId=PID/DC/HC08G&amp;amp;fromPSP=true&amp;amp;assetLockedForNavigation=true&amp;amp;componentId=2&amp;amp;leftNavCode=1&amp;amp;pageSize=25&amp;amp;Documentation=Documentation/00610Ksd1nd%60%60Data%20Sheets&amp;amp;fpsp=1&amp;amp;linkline=Data%20Sheets" rel="nofollow" target="_self"&gt;datasheet.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Section 18.3 Development Support/Monitor Module&lt;/P&gt;&lt;P&gt;Have a look in there and come back here if still unsure.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2011 03:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170602#M11412</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2011-09-29T03:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: mc68hc908gp32 bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170603#M11413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for your reply. I think that you are refering for figure 18-10 and figure 18-11. But the MCU is in circuit and it has a bootloader and a firmware. What I need it to stop the MCU to enter in bootloader to upload the firmware. I think that the circuit is not good for this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2011 04:17:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170603#M11413</guid>
      <dc:creator>mc68hc908</dc:creator>
      <dc:date>2011-09-29T04:17:59Z</dc:date>
    </item>
    <item>
      <title>Re: mc68hc908gp32 bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170604#M11414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mc68hc908,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, Peg was referring to that circuit and the "Monitor-Mode" bootloader that comes pre-programmed into the GP32.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your PCB does not have the circuit necessary, as shown in Figures 18-9, 18-10 and 18-11, then you can not use Monitor-Mode. Monitor-Mode is the &lt;EM&gt;only&lt;/EM&gt; bootloader that comes with the GP32.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are saying that your GP32 has an &lt;EM&gt;additional&lt;/EM&gt; bootloader that was installed with your original firmware, then you need to find the person who wrote it to find out how it is supposed to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Sep 2011 06:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908gp32-bootloader/m-p/170604#M11414</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2011-09-29T06:01:40Z</dc:date>
    </item>
  </channel>
</rss>