<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need to know about using the PTA2/KBIP2/CLK/nRst/VPP for input in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-know-about-using-the-PTA2-KBIP2-CLK-nRst-VPP-for-input/m-p/170561#M11397</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have literally tens of thousands of the MC9RS08KA2 in stock so Im trying to continue using it for a product upgrade. The problem that im facing is that i need one more input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My hope was to put two push buttons with in parallel on this pin. pusing one would give 0 volts and the second would give 2.5v and the pin would normall rest at 5 volts if no button was pressed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know that the reset can only be used as a Input but is is possible for it to detect different voltage levels?&lt;/P&gt;&lt;P&gt;PTA2/KBIP2/CLK/nRst/VPP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The IC will be pre programmed so I will not need the reset and or VPP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jun 2012 01:38:09 GMT</pubDate>
    <dc:creator>llester</dc:creator>
    <dc:date>2012-06-08T01:38:09Z</dc:date>
    <item>
      <title>Need to know about using the PTA2/KBIP2/CLK/nRst/VPP for input</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-know-about-using-the-PTA2-KBIP2-CLK-nRst-VPP-for-input/m-p/170561#M11397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have literally tens of thousands of the MC9RS08KA2 in stock so Im trying to continue using it for a product upgrade. The problem that im facing is that i need one more input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My hope was to put two push buttons with in parallel on this pin. pusing one would give 0 volts and the second would give 2.5v and the pin would normall rest at 5 volts if no button was pressed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know that the reset can only be used as a Input but is is possible for it to detect different voltage levels?&lt;/P&gt;&lt;P&gt;PTA2/KBIP2/CLK/nRst/VPP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The IC will be pre programmed so I will not need the reset and or VPP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2012 01:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-know-about-using-the-PTA2-KBIP2-CLK-nRst-VPP-for-input/m-p/170561#M11397</guid>
      <dc:creator>llester</dc:creator>
      <dc:date>2012-06-08T01:38:09Z</dc:date>
    </item>
    <item>
      <title>Re: Need to know about using the PTA2/KBIP2/CLK/nRst/VPP for input</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-know-about-using-the-PTA2-KBIP2-CLK-nRst-VPP-for-input/m-p/170562#M11398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;llester wrote:&lt;BR /&gt;&lt;P&gt;I know that the reset can only be used as a Input but is is possible for it to detect different voltage levels?&lt;/P&gt;&lt;P&gt;PTA2/KBIP2/CLK/nRst/VPP&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The short answer is no!&amp;nbsp; This input is only capable of detecting logic high or logic low levels.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your only hope would be to reallocate the comparator input&amp;nbsp;for the pair of switches (with the other input of the comparator connected to the bandgap), but this would only be likely to work for Vdd&amp;nbsp;5.0 volts.&amp;nbsp; The method will not work for Vdd 3.3 volts, and lower.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This&amp;nbsp;concept is to utilize the difference between logic low switching threshold (1.5 volts minimum @ 5V Vdd) and the bandgap reference voltage&amp;nbsp;(1.16-1.23 volts).&amp;nbsp; One of the switches must present an input level within the limits 1.23-1.5 volts, and the other switch an input level of less than 1.16 volts.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You would firstly sense that a logic low condition was present, and then enable the comparator input to determine which switch was the active one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2012 12:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-know-about-using-the-PTA2-KBIP2-CLK-nRst-VPP-for-input/m-p/170562#M11398</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-06-08T12:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: Need to know about using the PTA2/KBIP2/CLK/nRst/VPP for input</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-know-about-using-the-PTA2-KBIP2-CLK-nRst-VPP-for-input/m-p/170563#M11399</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Don't know how many buttons you already have but I have put three buttons on two inputs before.&lt;/P&gt;&lt;P&gt;It was up/down enter. Up and down where connected as normal and enter had a diode to both up and down.&lt;/P&gt;&lt;P&gt;When you got an input, straight after the debounce check for the other input, if it's on its enter or up/down if it's not.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2012 13:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-to-know-about-using-the-PTA2-KBIP2-CLK-nRst-VPP-for-input/m-p/170563#M11399</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2012-06-08T13:00:00Z</dc:date>
    </item>
  </channel>
</rss>