<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: USB Communication</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170480#M11373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a Card connected with an USB2.0 connector to a MotherBoard with an I3 processor.&lt;BR /&gt;My Card is realized around the S08JM60 Microcontroller.&lt;BR /&gt;Sometimes, the my card is not recognized by the Motherboard with the I3 processor.&lt;BR /&gt;I need to know, how can i detect, if my Card is connected or not connected?&lt;BR /&gt;Exactly, in which part in the Source code USB of the microcontroller S08 ?﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Oct 2011 22:26:27 GMT</pubDate>
    <dc:creator>OualBel</dc:creator>
    <dc:date>2011-10-04T22:26:27Z</dc:date>
    <item>
      <title>USB Communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170478#M11371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a card with S08JM60 Freescale microcontroller.&lt;/P&gt;&lt;P&gt;I have established a USB communication between my card and a Host PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Know, i neeed to add some code lines in order to give an information&lt;/P&gt;&lt;P&gt;when USB communication is not established&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Sep 2011 19:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170478#M11371</guid>
      <dc:creator>OualBel</dc:creator>
      <dc:date>2011-09-28T19:54:52Z</dc:date>
    </item>
    <item>
      <title>Re: USB Communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170479#M11372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sound like a self-powered device.&lt;/P&gt;&lt;P&gt;Assign a port pin to detect VBUS (5V) voltage at the USB connector.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tsuneo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2011 00:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170479#M11372</guid>
      <dc:creator>Tsuneo</dc:creator>
      <dc:date>2011-09-30T00:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: USB Communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170480#M11373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a Card connected with an USB2.0 connector to a MotherBoard with an I3 processor.&lt;BR /&gt;My Card is realized around the S08JM60 Microcontroller.&lt;BR /&gt;Sometimes, the my card is not recognized by the Motherboard with the I3 processor.&lt;BR /&gt;I need to know, how can i detect, if my Card is connected or not connected?&lt;BR /&gt;Exactly, in which part in the Source code USB of the microcontroller S08 ?﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Oct 2011 22:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170480#M11373</guid>
      <dc:creator>OualBel</dc:creator>
      <dc:date>2011-10-04T22:26:27Z</dc:date>
    </item>
    <item>
      <title>Re: USB Communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170481#M11374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Continue in your another post.&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="96766" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/96766" jivemacro="thread" title="https://community.freescale.com/thread/96766"&gt;https://community.freescale.com/thread/96766&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tsuneo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Oct 2011 21:26:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/USB-Communication/m-p/170481#M11374</guid>
      <dc:creator>Tsuneo</dc:creator>
      <dc:date>2011-10-06T21:26:42Z</dc:date>
    </item>
  </channel>
</rss>