<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: AW32 problems in 5V in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170454#M11368</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Are you sure that the whole chip is being supplied with 5V (including VDDAD)?&lt;BR /&gt;&lt;BR /&gt;The DS states that the maximum allowed difference between VDD and VDDAD is 100mV.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by fabio on &lt;SPAN class="date_text"&gt;2008-07-04&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:01 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Jul 2008 18:58:25 GMT</pubDate>
    <dc:creator>fabio</dc:creator>
    <dc:date>2008-07-04T18:58:25Z</dc:date>
    <item>
      <title>AW32 problems in 5V</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170451#M11365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi to all,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have made a little&amp;nbsp;LED blink application&amp;nbsp;for&amp;nbsp;the&amp;nbsp;AW32&amp;nbsp;MCU (MC9S08AW32 CFGE)&amp;nbsp;and programmed with the DEMOQE board through the BDM connector. I have tested the application with a supply voltage of 3.3V (BDM connector) and it works fine, but, when I supply the AW32 MCU with 5V (in other board with the LM2575-5.0)&amp;nbsp;the power supply enter in short circuit&amp;nbsp;(protection) and after some trys the AW32 MCU is damaged entering in internal short circuit (the BDM resets itself when I connect the MCU).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; My question is: the AW32 can&amp;nbsp;really use 5V as supply voltage? Does someone have made some project with the same components? What can be wrong?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2008 09:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170451#M11365</guid>
      <dc:creator>JohnnyS2K</dc:creator>
      <dc:date>2008-07-04T09:20:43Z</dc:date>
    </item>
    <item>
      <title>Re: AW32 problems in 5V</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170452#M11366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;The AW32 is good at 5V.&lt;BR /&gt;&lt;BR /&gt;Please be sure you did NOT connect VDD pin from the QE board.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2008 09:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170452#M11366</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-07-04T09:25:02Z</dc:date>
    </item>
    <item>
      <title>Re: AW32 problems in 5V</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170453#M11367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi JimDon,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I'm only connecting the VDD pin when I program the MCU, and in that way the MCU works, but when I disconnect the BDM cable and put the MCU on other board with a 5v supply then problem occurs.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2008 09:32:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170453#M11367</guid>
      <dc:creator>JohnnyS2K</dc:creator>
      <dc:date>2008-07-04T09:32:22Z</dc:date>
    </item>
    <item>
      <title>Re: AW32 problems in 5V</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170454#M11368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Are you sure that the whole chip is being supplied with 5V (including VDDAD)?&lt;BR /&gt;&lt;BR /&gt;The DS states that the maximum allowed difference between VDD and VDDAD is 100mV.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by fabio on &lt;SPAN class="date_text"&gt;2008-07-04&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:01 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2008 18:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170454#M11368</guid>
      <dc:creator>fabio</dc:creator>
      <dc:date>2008-07-04T18:58:25Z</dc:date>
    </item>
    <item>
      <title>Re: AW32 problems in 5V</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170455#M11369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Fábio,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp; The VSSAD, VDDAD, VREFL&amp;nbsp;and VREFH&amp;nbsp;are left unconnected in the same fashion as when I supply the MCU with the BDM connector. I will try to connect these pins to the respective signals and see if it works.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Johnny&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jul 2008 20:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170455#M11369</guid>
      <dc:creator>JohnnyS2K</dc:creator>
      <dc:date>2008-07-04T20:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: AW32 problems in 5V</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170456#M11370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Worked !!! If I connect the pins VSSAD, VDDAD, VREFL and VREFH to the respective signals the MCU works properly in 5V. Funny, in 3,3V these pins can be left unconnected without problems...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Johnny&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Jul 2008 04:58:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW32-problems-in-5V/m-p/170456#M11370</guid>
      <dc:creator>JohnnyS2K</dc:creator>
      <dc:date>2008-07-05T04:58:24Z</dc:date>
    </item>
  </channel>
</rss>