<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Internal Antenna Switch in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170418#M11362</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;With 1321x based boards if you want to use external antenna you can't enable it via software. By default SRB, NCB use circuit printed antenna. See this post for details: &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=8234" target="_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=8234&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Bye&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Dec 2007 18:41:22 GMT</pubDate>
    <dc:creator>CecchiSandrone</dc:creator>
    <dc:date>2007-12-05T18:41:22Z</dc:date>
    <item>
      <title>Internal Antenna Switch - MC1321X</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170417#M11361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi all&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Currently I am using a SRB (ZED) and NCB (ZC)&amp;nbsp;board. On both board, I am using the internal antenna switch instead of the external antenna switch. So i will like to find out what are the changes i need to make from&amp;nbsp;the freescale beekit?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I has try to generate out the solution from freescale beekit and I has change on the&amp;nbsp;option under the platform. I change the true to false for the use external antenna switch. However,&amp;nbsp;after i load the firmware to SRB board from freescale codewarrior, the SRB board didn't manage to transmit anything.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So maybe there&amp;nbsp;are more changes&amp;nbsp;needed to be made on the freescale beekit before loading it to the board. I not sure.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;trailrr&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Added p/n to subject&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2007-12-05&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;03:55 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2007 16:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170417#M11361</guid>
      <dc:creator>trailrr</dc:creator>
      <dc:date>2007-12-05T16:26:49Z</dc:date>
    </item>
    <item>
      <title>Re: Internal Antenna Switch</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170418#M11362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;With 1321x based boards if you want to use external antenna you can't enable it via software. By default SRB, NCB use circuit printed antenna. See this post for details: &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=8234" target="_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;thread.id=8234&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Bye&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2007 18:41:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170418#M11362</guid>
      <dc:creator>CecchiSandrone</dc:creator>
      <dc:date>2007-12-05T18:41:22Z</dc:date>
    </item>
    <item>
      <title>Re: Internal Antenna Switch</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170419#M11363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Please understand that there is a difference between using internal/external antenna switch and using either the PCB antenna or the SMA connector on the boards.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The SRB/NCB boards uses an external antenna switch, and the choice between the PCB and SMA is selected my moving a ZERO ohm resister.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;For you own hardware design you can choose between the internal or external antenna switch, and the software can be configured for this by&amp;nbsp;selecting&amp;nbsp;the user defined target and using the platform editor to select whether the software should configure the system for internal or external antenna switch.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Note that enabling internal antenna switch on the SRB/NCB board will make the RF not function properly.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;BR,&lt;/DIV&gt;&lt;DIV&gt;Mads&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2007 10:46:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170419#M11363</guid>
      <dc:creator>Mads</dc:creator>
      <dc:date>2007-12-07T10:46:32Z</dc:date>
    </item>
    <item>
      <title>Re: Internal Antenna Switch - MC1321X</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170420#M11364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;file MC1321XSRB:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;void RadioInit(void) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x11,0x80FF);&amp;nbsp;&amp;nbsp; /* Eliminate Unlock Conditions due to L01 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x1B,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC1. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x1D,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC2. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x1F,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC3. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x21,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC4. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x07,0x4C00);&amp;nbsp;&amp;nbsp; /* Enable CLKo in Doze&amp;nbsp; for externaal switch*/&lt;BR /&gt;.....&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;and&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;void RadioInit(void) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x11,0x80FF);&amp;nbsp;&amp;nbsp; /* Eliminate Unlock Conditions due to L01 */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x1B,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC1. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x1D,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC2. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x1F,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC3. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x21,0x8000);&amp;nbsp;&amp;nbsp; /* Disable TC4. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPIDrvWrite(0x07,&lt;STRONG&gt;0x5E00&lt;/STRONG&gt;);&amp;nbsp;&amp;nbsp; /* Enable CLKo in Doze for iinternaal switch*/&lt;BR /&gt;.....&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But I think that using external switch is the beest way to gain best radio-performance.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Dec 2007 04:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Internal-Antenna-Switch-MC1321X/m-p/170420#M11364</guid>
      <dc:creator>Alex_RUS</dc:creator>
      <dc:date>2007-12-11T04:52:31Z</dc:date>
    </item>
  </channel>
</rss>