<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックHow to stop flash erase operate in 9S08AW32?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-stop-flash-erase-operate-in-9S08AW32/m-p/170366#M11353</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;9S08AW32 need 20ms to earse a flash page, this is to long.&amp;nbsp; Is there some methos to&amp;nbsp;stop erase operate when a out&amp;nbsp;accident is happening ?I need return to run program in flash immediately .&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Dec 2007 10:47:33 GMT</pubDate>
    <dc:creator>wackestar</dc:creator>
    <dc:date>2007-12-05T10:47:33Z</dc:date>
    <item>
      <title>How to stop flash erase operate in 9S08AW32?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-stop-flash-erase-operate-in-9S08AW32/m-p/170366#M11353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;9S08AW32 need 20ms to earse a flash page, this is to long.&amp;nbsp; Is there some methos to&amp;nbsp;stop erase operate when a out&amp;nbsp;accident is happening ?I need return to run program in flash immediately .&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2007 10:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-stop-flash-erase-operate-in-9S08AW32/m-p/170366#M11353</guid>
      <dc:creator>wackestar</dc:creator>
      <dc:date>2007-12-05T10:47:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to stop flash erase operate in 9S08AW32?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-stop-flash-erase-operate-in-9S08AW32/m-p/170367#M11354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi wackestar,&lt;BR /&gt;I don't think you can do this!&lt;BR /&gt;If you can't tolerate the delay or can't only erase when you can then you need to use external EEPROM (IIC or SPI). Or change to a MPU with real EEPROM or two flash arrays.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2007 11:57:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-stop-flash-erase-operate-in-9S08AW32/m-p/170367#M11354</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-12-05T11:57:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to stop flash erase operate in 9S08AW32?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-stop-flash-erase-operate-in-9S08AW32/m-p/170368#M11355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;If you look in the MC9S08AW60 book, chapter 4.4.5 Access Errors, there are a number of things that will stop the erasure/programming execution.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I would try to write 0 into the FCBEF, which will cancel the command.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have not tried it myself, but it seems quite simple to try it.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2007 18:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-stop-flash-erase-operate-in-9S08AW32/m-p/170368#M11355</guid>
      <dc:creator>Ake</dc:creator>
      <dc:date>2007-12-05T18:32:46Z</dc:date>
    </item>
  </channel>
</rss>