<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Driving the segment LCD with MC9S08GT16 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Driving-the-segment-LCD-with-MC9S08GT16/m-p/169835#M11295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;Hello,&lt;BR /&gt;I've read about possibility of driving segment LCD display using any MCU with Analog-to-Digital Converter. It is simple and the only trick is to generate proper voltage sequence on ADC pins used as “COM” pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;To generate Vdd/2 necessary for the backplane a voltage divider is created using two equal sized pull-up and pull-down&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt; resistors on ADC pin. Whenever ADC(=COM) output pin on the microcontroller is set to analog in, this voltage divider provide necessery VDD/2 voltage to the LCD. Whenever the COM output pin is set to digital output 1 or 0 will be sent to LCD. The role of segment pins is performed by digital output pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I managed to display all icons on the LCD, but I have a problem with displaying single icons as the icons that should be dark is still visible, only less clearly. It is particularly evident when the small &lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;icon is to be displayed &lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and the neighbouring big icon should be invisible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I can see that connecting LCD display causes noise on the COM signals, looked as interference from other COMs and digital segments ( when I disconnect the display signals are free of noises).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Did anyone try to use segment LCD display with common MCU and know how to eliminate that problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marigold&lt;BR /&gt;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Jul 2008 13:48:04 GMT</pubDate>
    <dc:creator>marigold80</dc:creator>
    <dc:date>2008-07-03T13:48:04Z</dc:date>
    <item>
      <title>Driving the segment LCD with MC9S08GT16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Driving-the-segment-LCD-with-MC9S08GT16/m-p/169835#M11295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;Hello,&lt;BR /&gt;I've read about possibility of driving segment LCD display using any MCU with Analog-to-Digital Converter. It is simple and the only trick is to generate proper voltage sequence on ADC pins used as “COM” pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;To generate Vdd/2 necessary for the backplane a voltage divider is created using two equal sized pull-up and pull-down&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt; resistors on ADC pin. Whenever ADC(=COM) output pin on the microcontroller is set to analog in, this voltage divider provide necessery VDD/2 voltage to the LCD. Whenever the COM output pin is set to digital output 1 or 0 will be sent to LCD. The role of segment pins is performed by digital output pins.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I managed to display all icons on the LCD, but I have a problem with displaying single icons as the icons that should be dark is still visible, only less clearly. It is particularly evident when the small &lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;icon is to be displayed &lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and the neighbouring big icon should be invisible.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I can see that connecting LCD display causes noise on the COM signals, looked as interference from other COMs and digital segments ( when I disconnect the display signals are free of noises).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Did anyone try to use segment LCD display with common MCU and know how to eliminate that problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marigold&lt;BR /&gt;&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jul 2008 13:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Driving-the-segment-LCD-with-MC9S08GT16/m-p/169835#M11295</guid>
      <dc:creator>marigold80</dc:creator>
      <dc:date>2008-07-03T13:48:04Z</dc:date>
    </item>
    <item>
      <title>Re: Driving the segment LCD with MC9S08GT16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Driving-the-segment-LCD-with-MC9S08GT16/m-p/169836#M11296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;Hello,&lt;BR /&gt;if anyone is interested in solution of described problem: everything works just fine, the problem was caused by damaged heat seal connection of displays (floating COM signal).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;BR /&gt;Marigold&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jul 2008 15:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Driving-the-segment-LCD-with-MC9S08GT16/m-p/169836#M11296</guid>
      <dc:creator>marigold80</dc:creator>
      <dc:date>2008-07-11T15:02:54Z</dc:date>
    </item>
  </channel>
</rss>