<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Giber : McCarty node loses parent after Deep Sleep Wake up</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169515#M11243</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Elisa,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are right Set2Byte is made to copy 16 bit variable. But I don't know why it is not working in while copying the address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My working code looks like this&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void TxMyData()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; afAddrInfo_t afAddrInfo;&lt;BR /&gt;&amp;nbsp; zbNwkAddr_t DestNwkAddr = { 0X00, 0X00 };&lt;BR /&gt;&amp;nbsp; if (!mTxZigBeeThrottleFlag)&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; TS_SendEvent(gAppTaskID, mAppRetryZigBeeDataTx_c);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;BR /&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; FLib_MemSet(&amp;amp;afAddrInfo, 0, sizeof(afAddrInfo));&lt;BR /&gt;&amp;nbsp; zbTxDataBuffer.status = mBufStatusReadyToSend_c;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; afAddrInfo.aClusterId[0] = (mDataClusterId_c &amp;amp; 0xFF);&lt;BR /&gt;&amp;nbsp; afAddrInfo.aClusterId[1] = (mDataClusterId_c &amp;gt;&amp;gt; 8);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; afAddrInfo.dstAddrMode = gZbAddrMode16Bit_c;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; Copy2Bytes(afAddrInfo.dstAddr.aNwkAddr, DestNwkAddr);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; afAddrInfo.dstEndPoint = 0xff;&lt;BR /&gt;&amp;nbsp; afAddrInfo.srcEndPoint = appEndPoint;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; /* Turn on security and leave it on. Harmless In a non-secure network. */&lt;BR /&gt;&amp;nbsp; afAddrInfo.txOptions = 0;&lt;BR /&gt;&amp;nbsp; afAddrInfo.radiusCounter = afDefaultRadius_c;&lt;BR /&gt;&amp;nbsp; /* The Wireless UART application on the remote node will ack or nak this */&lt;BR /&gt;&amp;nbsp; /* datagram (regardless of the reliability mode setting), so a confirm id */&lt;BR /&gt;&amp;nbsp; /* is not needed here. */&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; AF_DataRequest(&amp;amp;afAddrInfo, zbTxDataBuffer.len, \&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; zbTxDataBuffer.data.structured.payload, NULL);&lt;BR /&gt;&amp;nbsp;......&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this may help you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Imran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Apr 2009 11:28:11 GMT</pubDate>
    <dc:creator>ImranChoudhary</dc:creator>
    <dc:date>2009-04-14T11:28:11Z</dc:date>
    <item>
      <title>ZigBee : MC1322x node loses parent after Deep Sleep Wake up</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169512#M11240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm working with &lt;SPAN style=": ; color: #000000; font-size: 2; font-family: Arial;"&gt;with codebase 3.0.1 and I have more or less the same problem: I want' my MC1322x ( chip version 2.0) Low Power Node goes to sleep and sends a test message to coordinator when it wake up. But sometimes, after wake up it loses its parents and like in you case "&lt;/SPAN&gt;&lt;SPAN style=": ; color: #000000; font-size: 2; font-family: Arial;"&gt;the led 1 blinking, and although I press the button 1 it remains blinking, it doesn´t make anything and it is imposible to&amp;nbsp;rejoin with the coordinator. What is happening?"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To send message I added&amp;nbsp; &lt;STRONG&gt;SendSampleMessage(TRUE);&lt;/STRONG&gt; in &lt;STRONG&gt;DeepSleepWakeupStackProc&lt;/STRONG&gt; function&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;/* Called each time deep sleep mode is exited. */&lt;BR /&gt;void DeepSleepWakeupStackProc&lt;BR /&gt;&amp;nbsp; (&lt;BR /&gt;&amp;nbsp; void&lt;BR /&gt;&amp;nbsp; )&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; TS_SendEvent(gAppTaskID, gAppEvtSyncReq_c);&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp; SendSampleMessage(TRUE);&lt;BR /&gt;&amp;nbsp; return;&lt;BR /&gt;}&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and defined this function in BeeApp.c&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;void SendSampleMessage(&amp;nbsp; bool_t wakeup)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; afAddrInfo_t afAddrInfo;&lt;BR /&gt;&amp;nbsp; FLib_MemSet(&amp;amp;afAddrInfo, 0, sizeof(afAddrInfo));&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; afAddrInfo.dstAddrMode = gZbAddrMode16Bit_c; /* direct-16 bit*/&lt;BR /&gt;&amp;nbsp; Set2Bytes(afAddrInfo.dstAddr.aNwkAddr, 0x0000); /* short address of coordinator */&lt;BR /&gt;&amp;nbsp; afAddrInfo.dstEndPoint = 0xFF;/*destination endpoint =0xFF : the receiving stack will deliver that message to every endpoint on the node*/&lt;BR /&gt;&amp;nbsp; Copy2Bytes(afAddrInfo.aClusterId, gZclClusterBinaryOutput_c);/* cluster to send it to */&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; afAddrInfo.srcEndPoint = appEndPoint;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; afAddrInfo.txOptions = gZclTxOptions;//0; /* to ACK or not to ACK, that is the question... */&lt;BR /&gt;&amp;nbsp; afAddrInfo.radiusCounter = afDefaultRadius_c; /* radius */&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; if (wakeup==FALSE)&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; AF_DataRequest( &amp;amp; afAddrInfo, 14, "\n Hello World\n" , NULL);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp; else&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; AF_DataRequest( &amp;amp; afAddrInfo, 14, "\n Goodmorning\n" , NULL);&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp; }&lt;BR /&gt;}&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Apr 2009 17:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169512#M11240</guid>
      <dc:creator>Elisa</dc:creator>
      <dc:date>2009-04-03T17:41:23Z</dc:date>
    </item>
    <item>
      <title>Re: Giber : McCarty node loses parent after Deep Sleep Wake up</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169513#M11241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Elisa,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is very annoying that we can't specify the destination address as in HEX formate directly it won't work out.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Actual problem is in the line&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Set2Bytes(afAddrInfo.dstAddr.aNwkAddr, 0x0000); /* short address of coordinator */&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To solve this problem you have to take the variable of type zbNwkAddr_t&lt;/P&gt;&lt;P&gt;ex: zbNwkAddr_t aDestAddress = {0x00, 0x00};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and use&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Copy2Bytes(afAddrInfo.dstAddr.aNwkAddr, aDestAddress);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This may solve the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheer.&lt;/P&gt;&lt;P&gt;Imran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2009 11:51:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169513#M11241</guid>
      <dc:creator>ImranChoudhary</dc:creator>
      <dc:date>2009-04-07T11:51:04Z</dc:date>
    </item>
    <item>
      <title>Re: Giber : McCarty node loses parent after Deep Sleep Wake up</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169514#M11242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Imram,&lt;/P&gt;&lt;P&gt;sorry but I'm not sure you are right. The Set2Byte function is made to copy a 16 bit variable to a location, with the bytes swapped if little endian, as you can see in &lt;SPAN&gt;BeeCommon.h&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;/*copies a 16 bit variable to a location with the bytes swapped&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; Note needed for big endian&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;*/&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#if !(gBigEndian_c)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void Set2Bytes(void *ptr, uint16_t val);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and it is used, as I used, FOR EXAMPLE in&amp;nbsp; &lt;SPAN&gt;ZdpUtils.c&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;void GetAddressFromService&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;case ZdoBackupBindingTableCache_c:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;if (!Cmp2BytesToZero(pPtr-&amp;gt;aServerMask))&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;Copy2Bytes(pNwkAddress, pPtr-&amp;gt;aNwkAddress);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;SPAN&gt;Set2Bytes(pNwkAddress, 0xffff);&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;break;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;default:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;SPAN&gt;Set2Bytes(pNwkAddress, 0xffff);&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;break;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However,I tried to follows your indication but the problem,as I thought, didn't solve.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;thanks anyway for your interest.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Bye,&lt;/DIV&gt;&lt;DIV&gt;Elisa&lt;BR /&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2009 16:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169514#M11242</guid>
      <dc:creator>Elisa</dc:creator>
      <dc:date>2009-04-07T16:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: Giber : McCarty node loses parent after Deep Sleep Wake up</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169515#M11243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Elisa,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are right Set2Byte is made to copy 16 bit variable. But I don't know why it is not working in while copying the address.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My working code looks like this&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;void TxMyData()&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; afAddrInfo_t afAddrInfo;&lt;BR /&gt;&amp;nbsp; zbNwkAddr_t DestNwkAddr = { 0X00, 0X00 };&lt;BR /&gt;&amp;nbsp; if (!mTxZigBeeThrottleFlag)&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; TS_SendEvent(gAppTaskID, mAppRetryZigBeeDataTx_c);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;BR /&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp; FLib_MemSet(&amp;amp;afAddrInfo, 0, sizeof(afAddrInfo));&lt;BR /&gt;&amp;nbsp; zbTxDataBuffer.status = mBufStatusReadyToSend_c;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; afAddrInfo.aClusterId[0] = (mDataClusterId_c &amp;amp; 0xFF);&lt;BR /&gt;&amp;nbsp; afAddrInfo.aClusterId[1] = (mDataClusterId_c &amp;gt;&amp;gt; 8);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; afAddrInfo.dstAddrMode = gZbAddrMode16Bit_c;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; Copy2Bytes(afAddrInfo.dstAddr.aNwkAddr, DestNwkAddr);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; afAddrInfo.dstEndPoint = 0xff;&lt;BR /&gt;&amp;nbsp; afAddrInfo.srcEndPoint = appEndPoint;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; /* Turn on security and leave it on. Harmless In a non-secure network. */&lt;BR /&gt;&amp;nbsp; afAddrInfo.txOptions = 0;&lt;BR /&gt;&amp;nbsp; afAddrInfo.radiusCounter = afDefaultRadius_c;&lt;BR /&gt;&amp;nbsp; /* The Wireless UART application on the remote node will ack or nak this */&lt;BR /&gt;&amp;nbsp; /* datagram (regardless of the reliability mode setting), so a confirm id */&lt;BR /&gt;&amp;nbsp; /* is not needed here. */&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; AF_DataRequest(&amp;amp;afAddrInfo, zbTxDataBuffer.len, \&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; zbTxDataBuffer.data.structured.payload, NULL);&lt;BR /&gt;&amp;nbsp;......&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this may help you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Imran&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2009 11:28:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-MC1322x-node-loses-parent-after-Deep-Sleep-Wake-up/m-p/169515#M11243</guid>
      <dc:creator>ImranChoudhary</dc:creator>
      <dc:date>2009-04-14T11:28:11Z</dc:date>
    </item>
  </channel>
</rss>