<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 MC9S08GT16A buffering inputs</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169312#M11203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello, I am using an MC9S08GT16A to interface with several 5v sensors. As such I need to buffer the inputs to make them 5v input tolorent.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am looking to use the 74LCX240 to buffer the inputs and was wondering if that was a good choice or if there are others I should use instead.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also can you recommend any bi directional buffers if I wanted to be able to change the&amp;nbsp;direction?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 02 Dec 2007 09:54:32 GMT</pubDate>
    <dc:creator>Kerms</dc:creator>
    <dc:date>2007-12-02T09:54:32Z</dc:date>
    <item>
      <title>MC9S08GT16A buffering inputs</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169312#M11203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello, I am using an MC9S08GT16A to interface with several 5v sensors. As such I need to buffer the inputs to make them 5v input tolorent.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am looking to use the 74LCX240 to buffer the inputs and was wondering if that was a good choice or if there are others I should use instead.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also can you recommend any bi directional buffers if I wanted to be able to change the&amp;nbsp;direction?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Dec 2007 09:54:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169312#M11203</guid>
      <dc:creator>Kerms</dc:creator>
      <dc:date>2007-12-02T09:54:32Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GT16A buffering inputs</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169313#M11204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Kerms,&lt;BR /&gt;&lt;BR /&gt;That part would seem to be OK.&lt;BR /&gt;Have you looked at &lt;A href="http://www.freescale.com/files/microcontrollers/doc/app_note/AN2433.pdf?fsrch=1" rel="nofollow" target="_blank"&gt;AN2433&lt;/A&gt;&lt;BR /&gt;SN74LVC1T45DBV is an example of a bi-directional buffer.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Dec 2007 10:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169313#M11204</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2007-12-02T10:47:04Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GT16A buffering inputs</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169314#M11205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Check out the ADI ADG330x family of parts.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.analog.com/en/prod/0,,767_828_ADG3304%2C00.html" target="test_blank"&gt;http://www.analog.com/en/prod/0,,767_828_ADG3304%2C00.html&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;They don't need directional pins.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by Witztronics on &lt;SPAN class="date_text"&gt;2007-12-01&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;10:45 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Dec 2007 11:44:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169314#M11205</guid>
      <dc:creator>Witztronics</dc:creator>
      <dc:date>2007-12-02T11:44:27Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GT16A buffering inputs</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169315#M11206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;If the sensors you refer to are the channel outputs from a RC receiver (as described in&amp;nbsp;another post), a satisfactory interface method may be to simply provide a series resistor (say 4k7)&amp;nbsp;for each input.&amp;nbsp; The intrinsic protection diodes will limit the voltage swing.&amp;nbsp; Alternatively, you could&amp;nbsp;add an external Schottky diode between each input (anode)&amp;nbsp;and +3V3 (cathode).&amp;nbsp; The external diode should conduct before the intrinsic diode does.&amp;nbsp; In both cases, the series resistor will limit current flow.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;A related method would be to provide a voltage divider to provide 3V3 output for an input of 5V.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;For any outputs from the MCU, you should first examine whether the external device will operate correctly with a 3V3 swing.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Dec 2007 15:10:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169315#M11206</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2007-12-02T15:10:33Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08GT16A buffering inputs</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169316#M11207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;I have used the following Tiny Logic part to succesfully interface +5v to +3.3v logic. The inputs&amp;nbsp;are 5 volt toleant when operating with a 3.3 volt supply.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;B&gt;&lt;FONT face="Arial" size="4"&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;P&gt;&lt;B&gt;&lt;FONT face="Arial" size="4"&gt;SN74LVC1G17&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;P&gt;&lt;B&gt;&lt;FONT face="Arial" size="4"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Dec 2007 16:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08GT16A-buffering-inputs/m-p/169316#M11207</guid>
      <dc:creator>Technoman64</dc:creator>
      <dc:date>2007-12-02T16:10:35Z</dc:date>
    </item>
  </channel>
</rss>