<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Help, 68HC908GZ60 interrupt vector under CodeWarrior</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-68HC908GZ60-interrupt-vector-under-CodeWarrior/m-p/168713#M11072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, given your description, I would suggest to fix this lack of manuals then first....&lt;BR /&gt;The device manuals can be downloaded from &lt;A href="http://www.freescale.com/"&gt;www.freescale.com&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code warrior manuals are under&lt;BR /&gt;C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.1\Help\PDF&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in case those are not installed, I would recommend to download the special edition installer and&lt;BR /&gt;reinstall it. Not sure if the manuals are separately download able too, could be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And about the actual question, the vector number 0 corresponds to the reset vector at address 0xFFFE, the vector 1 to the next vector at 0xFFFC, vector 2 to 0xFFFA,....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Jun 2008 07:52:21 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2008-06-28T07:52:21Z</dc:date>
    <item>
      <title>Help, 68HC908GZ60 interrupt vector under CodeWarrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-68HC908GZ60-interrupt-vector-under-CodeWarrior/m-p/168712#M11071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hello, I'm new here and unfortunately I'm new to CodeWarrior C programming for 68HC908GZ,,,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have to modify a project written by others, I can't find&amp;nbsp;an interrupt vector number table&amp;nbsp;for the declaration&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;interrupt &amp;lt;vector:number&amp;gt; void my_function()&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;In particular I'm interested in the serial (ESCI) receiver&amp;nbsp;/ transmitter / error interrupt vectors..&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Please don't tell me "look at the manual", the guy who wrote this program has left the company, all I have is his PC with CodeWarrior already installed and NO manual or help-file..&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks in advance&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Adolfo&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Jun 2008 06:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-68HC908GZ60-interrupt-vector-under-CodeWarrior/m-p/168712#M11071</guid>
      <dc:creator>la_panza</dc:creator>
      <dc:date>2008-06-28T06:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: Help, 68HC908GZ60 interrupt vector under CodeWarrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-68HC908GZ60-interrupt-vector-under-CodeWarrior/m-p/168713#M11072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, given your description, I would suggest to fix this lack of manuals then first....&lt;BR /&gt;The device manuals can be downloaded from &lt;A href="http://www.freescale.com/"&gt;www.freescale.com&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code warrior manuals are under&lt;BR /&gt;C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.1\Help\PDF&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in case those are not installed, I would recommend to download the special edition installer and&lt;BR /&gt;reinstall it. Not sure if the manuals are separately download able too, could be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And about the actual question, the vector number 0 corresponds to the reset vector at address 0xFFFE, the vector 1 to the next vector at 0xFFFC, vector 2 to 0xFFFA,....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Jun 2008 07:52:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-68HC908GZ60-interrupt-vector-under-CodeWarrior/m-p/168713#M11072</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2008-06-28T07:52:21Z</dc:date>
    </item>
  </channel>
</rss>