<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168685#M11048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the receive and transmit pins are both at 5V.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Dec 2010 23:47:06 GMT</pubDate>
    <dc:creator>Denikar</dc:creator>
    <dc:date>2010-12-10T23:47:06Z</dc:date>
    <item>
      <title>At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168681#M11044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to setup a CAN bus using a MC9S08DZ60 and the msCAN08 driver.&amp;nbsp; I have an 8MHz resonator and have msCAN08 configured (I think) for 250kbps, where the msCAN module is fed directly from the resonator.&amp;nbsp; The config portion is below:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*===========================================================================&lt;BR /&gt;&amp;nbsp;Define S08 msCAN module clock source: BUSCLK or MCGERCLK&lt;BR /&gt;&amp;nbsp;Permitted values: BUSCLK:&amp;nbsp;&amp;nbsp; Bus clock is used as clock source&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCGERCLK: Oscillator clock is used as clock source&lt;BR /&gt;===========================================================================*/&lt;BR /&gt;#define CLKSRC_CAN&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;MCGERCLK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;/*===========================================================================&lt;BR /&gt;&amp;nbsp;Define clock prescaler for msCAN module: permitted values 1 to 64&lt;BR /&gt;&amp;nbsp;msCAN module clock = CLKSRC_CAN / PRESCALER_CAN&lt;BR /&gt;===========================================================================*/&lt;BR /&gt;#define PRESCALER_CAN&amp;nbsp;&amp;nbsp; &amp;nbsp;4&lt;BR /&gt;/*===========================================================================&lt;BR /&gt;&amp;nbsp; Define msCAN module bit timing&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; Permitted values: PROP_SEG_CAN:&amp;nbsp;&amp;nbsp; 1 to 8 time quanta&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PHASE_SEG1_CAN: 1 to 8 time quanta&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PHASE_SEG2_CAN: 2, or PHASE_SEG1_CAN if greater&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; Bit time = (SYNC_SEG + PROP_SEG_CAN + PHASE_SEG1_CAN + PHASE_SEG2_CAN) * time quanta&lt;BR /&gt;&amp;nbsp; SYNC_SEG is always 1&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; Tq = 500nS with msCAN module fed from an 8MHz resonator, prescaler = 4&lt;BR /&gt;&amp;nbsp; Bit time = (1 + 1 + 3 + 3)*500nS = 250kbps&lt;BR /&gt;===========================================================================*/&lt;BR /&gt;#define PROP_SEG_CAN&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;1&lt;BR /&gt;#define PHASE_SEG1_CAN &amp;nbsp;&amp;nbsp; &amp;nbsp;3&lt;BR /&gt;#define PHASE_SEG2_CAN &amp;nbsp;&amp;nbsp; &amp;nbsp;3&lt;BR /&gt;/*===========================================================================&lt;BR /&gt;&amp;nbsp;Define msCAN module re-synchronisation jump width&lt;BR /&gt;&amp;nbsp;Permitted values: 1 to smaller of 4 and PHASE_SEG1_CAN time quanta&lt;BR /&gt;===========================================================================*/&lt;BR /&gt;#define RJW_CAN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;3&lt;BR /&gt;/*==========================================================================*/&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem is everytime I attempt to transmit I get a sync error, and see nothing on the scope.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Questions is given I need a 250kbps bus speed, do the settings above make sense?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Dec 2010 09:11:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168681#M11044</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-10T09:11:33Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168682#M11045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to BOSCH CAN specs (search for BCANSV2.0.pdf)&amp;nbsp; resonators may work up to 125kbps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the bus in&amp;nbsp;dominant&amp;nbsp; state?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Dec 2010 13:12:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168682#M11045</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-10T13:12:11Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168683#M11046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Good point.&amp;nbsp; I've tried many different speed configurations all with the same result.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No, the bus is not in the dominant state.&amp;nbsp; TxD stays at a constant 5V as I see nothing on it at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Dec 2010 22:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168683#M11046</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-10T22:11:05Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168684#M11047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It doesn't matter what you have on TxD. Do you have "1" on CAN receive pin? If not - you won't be able to send.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Dec 2010 22:56:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168684#M11047</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-10T22:56:27Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168685#M11048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the receive and transmit pins are both at 5V.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Dec 2010 23:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168685#M11048</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-10T23:47:06Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168686#M11049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;then something wrong must with your code&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Dec 2010 02:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168686#M11049</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-11T02:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168687#M11050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After further digging I'm finding the CAN bus isn't initializing properly at startup.&amp;nbsp; Freescale's CAN_Init function first calls a CAN_Reset function to soft reset the msCAN module.&amp;nbsp;&amp;nbsp; Below is a snippet of the first few lines of this function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;UINT8 CAN_Reset(UINT8 rmode)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;if (CANCTL1 &amp;amp; INITAK) return ERR_OK;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;STRONG&gt;&lt;FONT color="#333333"&gt;if (CANCTL0 &amp;amp; INITRQ) return ERR_INIT;&lt;/FONT&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;if (!((rmode == FAST) || (rmode == CMPTX)))&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;return (ERR_MODE);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This routine is called right out of reset AFTER initializing the system options register and clocks.&amp;nbsp; When it gets to the line in bold, it returns from the function and the CANCTL and config registers never get set.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now I need to figure out why the msCAN module is NOT in initialization mode right out of reset.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Dec 2010 21:33:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168687#M11050</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-11T21:33:16Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168688#M11051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After reading some additional posts I modified the code to do the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;&amp;nbsp; if (! (CANCTL0 &amp;amp; INITRQ))&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* If not in init mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CANCTL0 |= INITRQ;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enter&amp;nbsp; MSCAN initialization mode */&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp; while (!(CANCTL1 &amp;amp; INITAK));&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait until the MSCAN is in initialization mode */&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However the micro never will enter init mode and it loops endlessly on the while statement.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Dec 2010 00:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168688#M11051</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-12T00:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168689#M11052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you enable MSCAN (CANE bit)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Dec 2010 01:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168689#M11052</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-12T01:36:29Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168690#M11053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for all the replies.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the CANE bit is enabled just prior to the code snippet.&amp;nbsp; Here is the whole section:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;UINT8 CAN_Reset(UINT8 rmode)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; CANCTL1 |= 0x80;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable CAN (CANE bit) */&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; if (! (CANCTL0 &amp;amp; INITRQ))&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* If not in init mode */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CANCTL0 |= INITRQ;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enter&amp;nbsp; MSCAN initialization mode */&lt;BR /&gt;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp; while (!(CANCTL1 &amp;amp; INITAK));&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Wait until the MSCAN is in initialization mode */&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Dec 2010 01:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168690#M11053</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-12T01:53:55Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168691#M11054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hm, it should pass INITAK loop. Is oscilator&amp;nbsp;enabled and operating prior to CAN_Reset() call?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another reason to refuse to send may&amp;nbsp;be LISTEN bit. It is set by default.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is not cleat what's INITAK. Codewarrior headers don't have it defined. Is it bitmask or bit from CANCTL1 bitfield?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Dec 2010 03:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168691#M11054</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2010-12-12T03:13:17Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168692#M11055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Per your suggestion I added a line to clear the LISTEN bit, but it still gets stuck in the INITAK loop.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;INITAK is defined as 0x01.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes the oscillator is up and running prior to this.&amp;nbsp; All my timer interrupts are working fine.&amp;nbsp; However I'm beginning to think this problem is clock related.&amp;nbsp; I have the MCGERCLK enabled and am using that to feed the MSCAN module directly (CLKSRC bit in CANCTL1 set to 0). My timers all run off the PLL though.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Dec 2010 03:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168692#M11055</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-12T03:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: At wits end setting up CAN bus with msCAN08 driver on a MC9S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168693#M11056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Well I feel stupid.&amp;nbsp; Turns out the problem was caused from an uninitialized index.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In msCANreg.h the CAN registers are defined via a reference off CAN_BaseAddress:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;/******************************************************************************&lt;BR /&gt;&amp;nbsp;* msCAN module registers&lt;BR /&gt;&amp;nbsp;******************************************************************************/&lt;BR /&gt;#define CANCTL0 &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;(*((volatile UINT8&amp;nbsp; *const)(CAN_BaseAddress)))&lt;BR /&gt;#define CANCTL1 &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;(*((volatile UINT8&amp;nbsp; *const)(CAN_BaseAddress + 0x01)))&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I forgot to define it!&amp;nbsp; Duh!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the changes discussed in previous posts did need to be made.&amp;nbsp; Everything works fine now!&amp;nbsp; Thanks for all the help!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Dec 2010 09:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/At-wits-end-setting-up-CAN-bus-with-msCAN08-driver-on-a/m-p/168693#M11056</guid>
      <dc:creator>Denikar</dc:creator>
      <dc:date>2010-12-12T09:10:45Z</dc:date>
    </item>
  </channel>
</rss>