<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can JM60's S08ACMPV2 be used as a linear amplifier? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JM60-s-S08ACMPV2-be-used-as-a-linear-amplifier/m-p/167914#M10913</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, at least not as a standard opamp. The external signal ACMPO is a digital output, so it tends to slip either to Vdd or Vss depending on the actual analog level of ACMPO (internally). Thus you can't close the feedback via standard resistor network.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tested that, also wanted to use that opamp similarly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Feb 2010 04:45:02 GMT</pubDate>
    <dc:creator>ok2ucx</dc:creator>
    <dc:date>2010-02-05T04:45:02Z</dc:date>
    <item>
      <title>Can JM60's S08ACMPV2 be used as a linear amplifier?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JM60-s-S08ACMPV2-be-used-as-a-linear-amplifier/m-p/167913#M10912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Jan 2010 08:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JM60-s-S08ACMPV2-be-used-as-a-linear-amplifier/m-p/167913#M10912</guid>
      <dc:creator>z_george</dc:creator>
      <dc:date>2010-01-16T08:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can JM60's S08ACMPV2 be used as a linear amplifier?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JM60-s-S08ACMPV2-be-used-as-a-linear-amplifier/m-p/167914#M10913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, at least not as a standard opamp. The external signal ACMPO is a digital output, so it tends to slip either to Vdd or Vss depending on the actual analog level of ACMPO (internally). Thus you can't close the feedback via standard resistor network.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tested that, also wanted to use that opamp similarly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2010 04:45:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JM60-s-S08ACMPV2-be-used-as-a-linear-amplifier/m-p/167914#M10913</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2010-02-05T04:45:02Z</dc:date>
    </item>
    <item>
      <title>Re: Can JM60's S08ACMPV2 be used as a linear amplifier?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JM60-s-S08ACMPV2-be-used-as-a-linear-amplifier/m-p/167915#M10914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Pavel, thanks a lot for your information. I guess I mixed the MJ60 ACMPOV2 with Operational Amplifiers on MSP430Fxx. – The on chip Amplifier&amp;nbsp;is useful especially for sensor applications.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2010 05:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JM60-s-S08ACMPV2-be-used-as-a-linear-amplifier/m-p/167915#M10914</guid>
      <dc:creator>z_george</dc:creator>
      <dc:date>2010-02-05T05:26:47Z</dc:date>
    </item>
  </channel>
</rss>