<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S08QE32 load capacitors in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE32-load-capacitors/m-p/167583#M10828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora mlun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As an example the DEMOQE board's schematic shows 22pF caps on xtal.&lt;/P&gt;&lt;P&gt;On my board there are no caps fitted, No Rf and Rs is zero ohms.&lt;/P&gt;&lt;P&gt;The manual does say in several places that this is correct for low range/low power mode.&lt;/P&gt;&lt;P&gt;Have not actually run external oscillator myself.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 29 Mar 2009 05:41:41 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2009-03-29T05:41:41Z</dc:date>
    <item>
      <title>S08QE32 load capacitors</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE32-load-capacitors/m-p/167582#M10827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm about to try the QE32 with external 32kHz&amp;nbsp;crystal RANGE=HGO=0.&lt;/P&gt;&lt;P&gt;The datasheet says that the load capacitors and series resistor&amp;nbsp;are incorporated, but I can't find any recommendations for the crystals load capacitance.&lt;/P&gt;&lt;P&gt;Common 32kHz crystals have load capacitance 6-12pF.&lt;/P&gt;&lt;P&gt;Which load capacitance is best?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Magnus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Mar 2009 19:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE32-load-capacitors/m-p/167582#M10827</guid>
      <dc:creator>mlun</dc:creator>
      <dc:date>2009-03-28T19:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: S08QE32 load capacitors</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE32-load-capacitors/m-p/167583#M10828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora mlun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As an example the DEMOQE board's schematic shows 22pF caps on xtal.&lt;/P&gt;&lt;P&gt;On my board there are no caps fitted, No Rf and Rs is zero ohms.&lt;/P&gt;&lt;P&gt;The manual does say in several places that this is correct for low range/low power mode.&lt;/P&gt;&lt;P&gt;Have not actually run external oscillator myself.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Mar 2009 05:41:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE32-load-capacitors/m-p/167583#M10828</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-03-29T05:41:41Z</dc:date>
    </item>
  </channel>
</rss>