<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックDEMOQE BDM Functionality questions</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166927#M10711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I bought one of the DEMOQE boards made by P&amp;amp;E and distributed by mouser et. al for $50.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is, if I install the 6-pin header and use this board to program external target boards, will it support voltage level translation for, lets say a AW32 processor running at 5V.&amp;nbsp; The QE board runs at roughly 3 Volts, but it does have a battery to power the board from, so I would assume this would mean that the USB-BDM that is on the backside of the board would have to have some kind of level translation to allow the variable voltage.&amp;nbsp; I'm just not sure how high this can go.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Would appreciate any advice.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Aaron&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jun 2008 22:14:38 GMT</pubDate>
    <dc:creator>protoease</dc:creator>
    <dc:date>2008-06-23T22:14:38Z</dc:date>
    <item>
      <title>DEMOQE BDM Functionality questions</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166927#M10711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I bought one of the DEMOQE boards made by P&amp;amp;E and distributed by mouser et. al for $50.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is, if I install the 6-pin header and use this board to program external target boards, will it support voltage level translation for, lets say a AW32 processor running at 5V.&amp;nbsp; The QE board runs at roughly 3 Volts, but it does have a battery to power the board from, so I would assume this would mean that the USB-BDM that is on the backside of the board would have to have some kind of level translation to allow the variable voltage.&amp;nbsp; I'm just not sure how high this can go.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Would appreciate any advice.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Aaron&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2008 22:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166927#M10711</guid>
      <dc:creator>protoease</dc:creator>
      <dc:date>2008-06-23T22:14:38Z</dc:date>
    </item>
    <item>
      <title>Re: DEMOQE BDM Functionality questions</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166928#M10712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;I have it used to to debug +5 V hcs12 boards. So I would say yes. Needless to say to NOT connect the VSS pin.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jun 2008 23:30:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166928#M10712</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-06-23T23:30:22Z</dc:date>
    </item>
    <item>
      <title>Re: DEMOQE BDM Functionality questions</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166929#M10713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Finally tried it out, I just installed 5 pins the 6 pin BDM header onto the DEMOQE board (I didn't install a pin in the VDD line) and it programmed and debugged my protoboard built QG8 prototype just fine.&lt;BR /&gt;&lt;BR /&gt;This is a good way to get what seems to be the full functionality of the PE BDM pod at about half the cost.&amp;nbsp; The only thing in my mind that you are lacking is a nice case.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Aug 2008 19:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166929#M10713</guid>
      <dc:creator>protoease</dc:creator>
      <dc:date>2008-08-20T19:19:24Z</dc:date>
    </item>
    <item>
      <title>Re: DEMOQE BDM Functionality questions</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166930#M10714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;It also can not program the KA series, because it needs 12v vpp. Supposedly it is also not as well protected as the USB Mulitlink.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Aug 2008 20:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166930#M10714</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-08-20T20:59:36Z</dc:date>
    </item>
    <item>
      <title>Re: DEMOQE BDM Functionality questions</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166931#M10715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Just wanted to know if you were able to get the DEMOQE to program an external MCF51QE128 via the BDM connector.&lt;/P&gt;&lt;P&gt;Thanks for any help.&lt;/P&gt;&lt;P&gt;Ada,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Apr 2011 22:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMOQE-BDM-Functionality-questions/m-p/166931#M10715</guid>
      <dc:creator>BobbyMK</dc:creator>
      <dc:date>2011-04-07T22:25:03Z</dc:date>
    </item>
  </channel>
</rss>