<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックErrors when programming in C++</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Errors-when-programming-in-C/m-p/166830#M10704</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to create a program in C++&amp;nbsp;in Code Warrior for MC9S08SE8.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This software has already been created and tested for other uc (and another IDE).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I create it in Code Warrior, several errors have been appeared.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Examples:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) C1007: Type specifier mismatch&lt;/P&gt;&lt;P&gt;2) C5002: Illegal type&lt;/P&gt;&lt;P&gt;3) C1432: No valid classname specified&lt;/P&gt;&lt;P&gt;4) C1815: getInstance not declared&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone can help me, I can send the project with the files created (for more details). &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you, in advance.&lt;/P&gt;&lt;P&gt;Raphael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jan 2010 02:50:27 GMT</pubDate>
    <dc:creator>cremonezi</dc:creator>
    <dc:date>2010-01-13T02:50:27Z</dc:date>
    <item>
      <title>Errors when programming in C++</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Errors-when-programming-in-C/m-p/166830#M10704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to create a program in C++&amp;nbsp;in Code Warrior for MC9S08SE8.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This software has already been created and tested for other uc (and another IDE).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I create it in Code Warrior, several errors have been appeared.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Examples:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) C1007: Type specifier mismatch&lt;/P&gt;&lt;P&gt;2) C5002: Illegal type&lt;/P&gt;&lt;P&gt;3) C1432: No valid classname specified&lt;/P&gt;&lt;P&gt;4) C1815: getInstance not declared&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone can help me, I can send the project with the files created (for more details). &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you, in advance.&lt;/P&gt;&lt;P&gt;Raphael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2010 02:50:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Errors-when-programming-in-C/m-p/166830#M10704</guid>
      <dc:creator>cremonezi</dc:creator>
      <dc:date>2010-01-13T02:50:27Z</dc:date>
    </item>
    <item>
      <title>Re: Errors when programming in C++</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Errors-when-programming-in-C/m-p/166831#M10705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which edition of CodeWarrior are you using? Special edition= Standard Edition? Professional edition?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to be able to use C++ you need a professional edition.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also keep in mind that you have limited RAM and ROM resources available on a HC08 microcontroller. Full C++ support is not available on this architecture.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is supported here is more embedded C++ than full C++.&lt;/P&gt;&lt;P&gt;Some feature of C++ are not supported in embedded C++.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to allow us to investigate what is going on here, I would recommend you to submit a service request for that.&lt;BR /&gt;&lt;BR /&gt;Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework?regFlag=fromOpenSR" rel="nofollow" target="_blank"&gt;here&lt;/A&gt; to submit a service request.&lt;BR /&gt;&lt;BR /&gt;Make sure to attach a reproducible project and installed product information to the service request.&lt;BR /&gt;To generate the required information:&lt;BR /&gt;- Start CodeWarrior&lt;BR /&gt;- Open the project&lt;BR /&gt;- Select "Help" -&amp;gt; "Pack and Go" and follow instructions on the screen.&lt;BR /&gt;&lt;BR /&gt;Attach the generated .zip file to the SR.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2010 07:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Errors-when-programming-in-C/m-p/166831#M10705</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-01-13T07:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: Errors when programming in C++</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Errors-when-programming-in-C/m-p/166832#M10706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the installation CD box, there is: "CodeWarrior Development Studio for Microcontrollers Special Edition and HCS12(X) Special Edition". Then, no Professional edition, isn't?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway, I will submit a service request with the project in order to you know the errors...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Cremonezi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2010 18:38:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Errors-when-programming-in-C/m-p/166832#M10706</guid>
      <dc:creator>cremonezi</dc:creator>
      <dc:date>2010-01-13T18:38:20Z</dc:date>
    </item>
  </channel>
</rss>