<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166565#M10647</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon, i´ve programed the jm60 and then i supossed erased the bootloader rutine because the fresscale jm60 Gui doesn´t work. How I can to program the bootloader on the jm60 again?. Thanks a lot for your possible help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 17 Oct 2010 22:19:09 GMT</pubDate>
    <dc:creator>eigic245</dc:creator>
    <dc:date>2010-10-17T22:19:09Z</dc:date>
    <item>
      <title>Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166558#M10640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I Im trying to use Processor Expert and the AN3561 USB Bootloader but every time I try I get compile errors. I am able to make programs without PE and tun them with bootloader, but when I try to Enable PE in that same proyect it all messes up. How can I do it ?&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2010 18:01:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166558#M10640</guid>
      <dc:creator>carloscuevas</dc:creator>
      <dc:date>2010-01-11T18:01:01Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166559#M10641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;please find attached two projects that show a bootloader and a test application within Processor Expert using the library described in AN3561. The PE_bootloader project PE_bootloader_AN3561.mcp re-uses example from AN3561. The PE_bootloader_AN3561_blink.mcp project is a test application for bootloader.&lt;BR /&gt;&lt;BR /&gt;The PE_bootloader_AN3561 project conatins bootloader and simple application code that just switches the LED on in case that bootloader mode is not entered. After uploading a new program (the PE_bootloader_AN3561_blink project) and resetting the MCU, the LED on PTE2 starts blinking at 10Hz frequency. For more details please see the readme.txt file enclosed in projects.&lt;BR /&gt;You can simple extend bootloader and application projects with additional beans according to your requiremets.&lt;BR /&gt;&lt;BR /&gt;Note:&lt;BR /&gt;There is possible to have the bootloader and the application integrated in one project. Separate programming of bootloader and application are not required in this case. Disadvantage of this solution&lt;BR /&gt;is that generation of prm file by PE must be disabled and distributed binary code always contains bootloader.&lt;BR /&gt;&lt;BR /&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Feb 2010 23:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166559#M10641</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2010-02-08T23:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166560#M10642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thank you very much&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Feb 2010 00:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166560#M10642</guid>
      <dc:creator>carloscuevas</dc:creator>
      <dc:date>2010-02-09T00:14:09Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166561#M10643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!!!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Feb 2010 08:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166561#M10643</guid>
      <dc:creator>thinkchip</dc:creator>
      <dc:date>2010-02-21T08:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166562#M10644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Trying not to be to overbearing..........&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please do not thank people by adding more posts to a thread. The whole world does not want to log on to a technical forum to read post that just say "thanks".&lt;/P&gt;&lt;P&gt;The correct/polite way to do it is to rate their post and/or correctly mark THEIR post as a solution. There has been quite a few instances where people have marked their own "thank you" post as the "solution" (Two no-no's in the one post!)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2010 06:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166562#M10644</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-02-23T06:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166563#M10645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok peg I understand your point. I know you're just trying to make this forum a better place. Im sorry for being such an annoying member&amp;nbsp; &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2010 10:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166563#M10645</guid>
      <dc:creator>carloscuevas</dc:creator>
      <dc:date>2010-02-23T10:41:26Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166564#M10646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually it seems that our &lt;A href="https://community.freescale.com/message/62528#62528" title="https://community.freescale.com/message/62528#62528"&gt;https://community.freescale.com/message/62528#62528&lt;/A&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Feb 2010 14:44:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166564#M10646</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-02-23T14:44:24Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166565#M10647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon, i´ve programed the jm60 and then i supossed erased the bootloader rutine because the fresscale jm60 Gui doesn´t work. How I can to program the bootloader on the jm60 again?. Thanks a lot for your possible help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Oct 2010 22:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166565#M10647</guid>
      <dc:creator>eigic245</dc:creator>
      <dc:date>2010-10-17T22:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166566#M10648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning, i`ve got a JM60 with bootloader. How I can to delete bootloader because i would like to use the ptg0 ptg1 ports?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot for your kind answers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Oct 2010 22:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166566#M10648</guid>
      <dc:creator>eigic245</dc:creator>
      <dc:date>2010-10-20T22:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166567#M10649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I didn´t erase the bootloader, excusme please&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Oct 2010 22:51:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166567#M10649</guid>
      <dc:creator>eigic245</dc:creator>
      <dc:date>2010-10-20T22:51:58Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166568#M10650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The link is broken, could you provided again?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2015 02:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166568#M10650</guid>
      <dc:creator>brauliochisalav</dc:creator>
      <dc:date>2015-10-22T02:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166569#M10651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please find the original projects in attached archive. It was lost during former forum transition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2015 08:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166569#M10651</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2015-10-22T08:00:25Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166570#M10652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any chance to upload this examples to codewarrior 10.x??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 May 2016 19:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166570#M10652</guid>
      <dc:creator>brauliochisalav</dc:creator>
      <dc:date>2016-05-06T19:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: Processor Expert and AN3561SW JM60 USB Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166571#M10653</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;not sure if this will work, but you can try to create new project for the same CPU and overwrite the ProcesorExpert.pe file in new project by using the *.pe file from zip (I recommend to close CW (or project in workspace) before this operation).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: *.pe file contains only settings for Processor Expert = only generate file will be affected the rest must be ported manually.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;Vojtech Filip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 07:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Processor-Expert-and-AN3561SW-JM60-USB-Bootloader/m-p/166571#M10653</guid>
      <dc:creator>vfilip</dc:creator>
      <dc:date>2016-05-09T07:13:25Z</dc:date>
    </item>
  </channel>
</rss>