<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Bootloader questions for HCS08AW</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-questions-for-HCS08AW/m-p/166437#M10622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can only comment on the first part of your questions.&lt;/P&gt;&lt;P&gt;The ILLEGAL_BP is normal when running the bootloader with the BDM.&lt;/P&gt;&lt;P&gt;When using the BDM it halts on errors such as the ILLEGAL_BP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You need to have the pc program running before you run the bootloader program in the micro otherwise the bootloader will timeout and cause a illegal operation to force a reboot which normally would allow the micro to start running your code if it were in the micro.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other things i can think of that could cause probles are:&lt;/P&gt;&lt;P&gt;How do you have the PC serial port connected to the micro?&lt;/P&gt;&lt;P&gt;What serial port are you using in the micro to connect to the serial port on the PC?&lt;/P&gt;&lt;P&gt;Did you complile the bootloader to use the correct serial port in the micro?&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by RWalker on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-03-26&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;08:48 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2009 22:43:32 GMT</pubDate>
    <dc:creator>RWalker</dc:creator>
    <dc:date>2009-03-26T22:43:32Z</dc:date>
    <item>
      <title>Bootloader questions for HCS08AW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-questions-for-HCS08AW/m-p/166436#M10621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a bootloader for field upgrading of my MC9S08AW32 app and have some questions.&amp;nbsp; I have read AN2295 and have built the latest project for the 9S08.&lt;/P&gt;&lt;P&gt;For starters I just built the bootloader and tried to establish communication with the master gui app.&lt;/P&gt;&lt;P&gt;1) The bootloader builds, but when I try to load and run it using a P&amp;amp;E Multilink BDM, it breaks, with the following displayed in the command window:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Frequency change to ~7902832hz.&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;Frequency change to ~3790830hz.&lt;BR /&gt;ILLEGAL_BP&lt;/P&gt;&lt;P&gt;in&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I&amp;nbsp;started the master gui app and it runs and displays:&lt;/P&gt;&lt;P&gt;Parsed S-record lines: 220&amp;nbsp;&amp;nbsp; Bytes total:6873&lt;/P&gt;&lt;P&gt;Source address range: 0x8000-0xFFFF&lt;/P&gt;&lt;P&gt;Waiting for HS(S)08 reset ACK...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Restarting the BDM still does not change the above behavior&lt;/P&gt;&lt;P&gt;1) What do I need to do to get it to run?&lt;/P&gt;&lt;P&gt;2) Inspecting the included mc9s08aw60.prm, there are lines&lt;/P&gt;&lt;P&gt;&amp;nbsp; NVPROTROM = READ_ONLY 0xFFBD TO 0xFFBD;&lt;BR /&gt;&amp;nbsp; NVOPTROM&amp;nbsp; = READ_ONLY 0xFFBF TO 0xFFBF;&lt;BR /&gt;I was expecting these to be set to protect the bootloader.&amp;nbsp; What do there parameters have to be to protect the bootloader, while implementing the interrupt vector re-mapping?&lt;/P&gt;&lt;P&gt;3) If I want to build the bootloader into my app so that it will be loaded as a single file, what changes to the interrupt vector table or other changes to the prm file have to be accomplished, and still be compatible with the initializer?&lt;/P&gt;&lt;P&gt;My current&amp;nbsp;.prm file is:&lt;/P&gt;&lt;P&gt;SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Z_RAM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_WRITE&amp;nbsp;&amp;nbsp; 0x0070 TO 0x00FF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; RAM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_WRITE&amp;nbsp;&amp;nbsp; 0x0100 TO 0x086F;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_ONLY&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x8000 TO 0xFF8F;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_ONLY&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xFF90 TO 0xFFCB;&lt;BR /&gt;&amp;nbsp;/* INTVECTS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; =&amp;nbsp; READ_ONLY&amp;nbsp;&amp;nbsp;&amp;nbsp; 0xFFCC TO 0xFFFF; Reserved for Interrupt Vectors */&lt;BR /&gt;END&lt;/P&gt;&lt;P&gt;PLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEFAULT_RAM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* non-zero page variables */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTO&amp;nbsp; RAM;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _PRESTART,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* startup code */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STARTUP,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* startup data structures */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ROM_VAR,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* constant variables */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; STRINGS,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* string literals */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; VIRTUAL_TABLE_SEGMENT,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* C++ virtual table segment */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DEFAULT_ROM,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; COPY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* copy down information: how to initialize variables */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTO&amp;nbsp; ROM; /* ,ROM1: To use "ROM1" as well, pass the option -OnB=b to the compiler */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _DATA_ZEROPAGE,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* zero page variables */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; MY_ZEROPAGE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; INTO&amp;nbsp; Z_RAM;&lt;BR /&gt;END&lt;/P&gt;&lt;P&gt;STACKSIZE 0x400&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//VECTOR 0 _Startup&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Reset vector: this is the default entry point for an application. */&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4) For the MC9S08AW32, is the&amp;nbsp;"FC Protocol, Version 2, HC9S08", the applicable version?&lt;/P&gt;&lt;P&gt;5) When using a 16 Mhz external oscillator, and ICG, is there still the ability to trim the baud rate clock?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2009 01:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-questions-for-HCS08AW/m-p/166436#M10621</guid>
      <dc:creator>jerryn</dc:creator>
      <dc:date>2009-03-25T01:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader questions for HCS08AW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-questions-for-HCS08AW/m-p/166437#M10622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can only comment on the first part of your questions.&lt;/P&gt;&lt;P&gt;The ILLEGAL_BP is normal when running the bootloader with the BDM.&lt;/P&gt;&lt;P&gt;When using the BDM it halts on errors such as the ILLEGAL_BP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You need to have the pc program running before you run the bootloader program in the micro otherwise the bootloader will timeout and cause a illegal operation to force a reboot which normally would allow the micro to start running your code if it were in the micro.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other things i can think of that could cause probles are:&lt;/P&gt;&lt;P&gt;How do you have the PC serial port connected to the micro?&lt;/P&gt;&lt;P&gt;What serial port are you using in the micro to connect to the serial port on the PC?&lt;/P&gt;&lt;P&gt;Did you complile the bootloader to use the correct serial port in the micro?&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by RWalker on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-03-26&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;08:48 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2009 22:43:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-questions-for-HCS08AW/m-p/166437#M10622</guid>
      <dc:creator>RWalker</dc:creator>
      <dc:date>2009-03-26T22:43:32Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader questions for HCS08AW</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-questions-for-HCS08AW/m-p/166438#M10623</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply.&amp;nbsp; Yes, I needed to start the download app and select the download file....I got it to work, and found a few other details with my app that may need to be changed, as it includes writing to flash, which is the only part that seems to break versus a directly loaded version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jerry&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2009 23:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-questions-for-HCS08AW/m-p/166438#M10623</guid>
      <dc:creator>jerryn</dc:creator>
      <dc:date>2009-03-26T23:51:34Z</dc:date>
    </item>
  </channel>
</rss>