<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: problems with USB power when using ADC 12bit in JM Family in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164972#M10342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the tip, but I use the Demo Board for a quick prototype to see if it works, then I will create an embedded board avoiding the Demo. Even that, the ADR444BRZ has 1,6mv tolerance (including temperature, etc.. ) . Dont know nothing about that you say, I will try to read something about that if I encounter that, but I have already bought the chip and I will tell you how it works in a few hours &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Dec 2010 22:27:01 GMT</pubDate>
    <dc:creator>Betadine</dc:creator>
    <dc:date>2010-12-01T22:27:01Z</dc:date>
    <item>
      <title>problems with USB power when using ADC 12bit in JM Family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164967#M10337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;3 weeks ago I posted questions about which Micro use for 12 bit ADC conversions. I chose JM family and we spoke about the problems I would found in 12bit conversions, specially Mac who post some design issues &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fthread%2F71136" rel="nofollow" target="_blank"&gt;steps:&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fthread%2F71136" rel="nofollow" target="_blank"&gt;Well&lt;/A&gt;! Im running with a JMDemo Board, 12bit ADC, and reading the values in Excel, I take an average of 50 values and it works fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Problem: Instability in Vcc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no noise in the data signals, all works better than good, but the problem is that I take the power from the USB, and when I looked with the Multimeter I realized why the values moves a little in the ADC. Is the USB Power!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, Data acquisition units that take the power from the USB... what they do? Can anyone shed some light in this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The goal is to stabilize the 5V USB Power signal, but I dont know any common method to do it.&lt;/P&gt;&lt;P&gt;Do I need to reduce to around 3V to stabilize it? (cause the stabilizer chip)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What do you think?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cristian.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Nov 2010 22:23:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164967#M10337</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-11-24T22:23:39Z</dc:date>
    </item>
    <item>
      <title>Re: problems with USB power when using ADC 12bit in JM Family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164968#M10338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, it seems that a voltage reference fit this need.&lt;/P&gt;&lt;P&gt;Specially the ADR444BRZ from analog devices, Vout = 4096V with an impressive max tolerance of 1.6mv totally independent of temperature.&lt;/P&gt;&lt;P&gt;DS speaks about using this in PCMCIA and data adquisition units with ADCs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Nov 2010 00:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164968#M10338</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-11-26T00:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: problems with USB power when using ADC 12bit in JM Family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164969#M10339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Cristian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are correct about using an external voltage reference to provide the required reference stability.&amp;nbsp; However, check that&amp;nbsp;its minimum supply voltage, assuming&amp;nbsp;a three-terminal device, is less than the minimum Vdd for the MCU, presumably about 4.5 volts.&amp;nbsp; You should also take into account any noise fluctuations that may occur on the Vdd line.&amp;nbsp; If the reference&amp;nbsp;drop out voltage is too high, a lower reference voltage might need to be chosen.&amp;nbsp; The minimum allowable&amp;nbsp;is 2.7 volt.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Nov 2010 02:43:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164969#M10339</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-11-27T02:43:54Z</dc:date>
    </item>
    <item>
      <title>Re: problems with USB power when using ADC 12bit in JM Family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164970#M10340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the chip I have posted has&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Vin: 4.5 - 12 volts&lt;/P&gt;&lt;P&gt;Vout: 4V&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;USB power: 5V&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So the reference voltage is only applied to pin VrefADC of the micro, the rest take the power directly from the USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It will work then with 0-4V for the ADC... it can be tweaked in the source. It must be work by that way.&lt;/P&gt;&lt;P&gt;The rest of the signals has no noise.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;USB Power must be higher than 4.5V... that´s the only dangerous requirement, I think it will work... well "it should work"! jeje. Hope not to encounter any trouble with it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All the Best.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cristian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Nov 2010 17:59:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164970#M10340</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-11-27T17:59:19Z</dc:date>
    </item>
    <item>
      <title>Re: problems with USB power when using ADC 12bit in JM Family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164971#M10341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you aware that the JM60 has a bandgap voltage reference on board?&lt;/P&gt;&lt;P&gt;Unfortunately, this can' t be used as reference for the ADC, but you may be able to use a sequence like that:&lt;/P&gt;&lt;P&gt;&amp;nbsp;- read bandgap&lt;/P&gt;&lt;P&gt;&amp;nbsp;- read signal&lt;/P&gt;&lt;P&gt;&amp;nbsp;- read bandgap&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From the bandgap reading, you can calculate the current supply/reference voltage.&lt;/P&gt;&lt;P&gt;If it does not change too fast, you may get the required accuracy from this approach.&lt;/P&gt;&lt;P&gt;(Having a bandgap but not being able to use it as ADC reference directly is something that I never understood...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dietmar&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 27 Nov 2010 21:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164971#M10341</guid>
      <dc:creator>dschwertb1</dc:creator>
      <dc:date>2010-11-27T21:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: problems with USB power when using ADC 12bit in JM Family</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164972#M10342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the tip, but I use the Demo Board for a quick prototype to see if it works, then I will create an embedded board avoiding the Demo. Even that, the ADR444BRZ has 1,6mv tolerance (including temperature, etc.. ) . Dont know nothing about that you say, I will try to read something about that if I encounter that, but I have already bought the chip and I will tell you how it works in a few hours &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Dec 2010 22:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problems-with-USB-power-when-using-ADC-12bit-in-JM-Family/m-p/164972#M10342</guid>
      <dc:creator>Betadine</dc:creator>
      <dc:date>2010-12-01T22:27:01Z</dc:date>
    </item>
  </channel>
</rss>