<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need help on using ADC interrupt for a simple operation - MC9S08AW60 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-help-on-using-ADC-interrupt-for-a-simple-operation/m-p/164893#M10336</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've got it working already. The error was due to&amp;nbsp;some extra code in the for(;; ) loop, which I didn't include here. Thx&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Mar 2009 11:03:57 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2009-03-23T11:03:57Z</dc:date>
    <item>
      <title>Need help on using ADC interrupt for a simple operation - MC9S08AW60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-help-on-using-ADC-interrupt-for-a-simple-operation/m-p/164892#M10335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I'm using MC9S08AW60 MCU and I've just started using ADC. So I'm starting out by doing a simple operation. It involves an infrared sensor which is connected to the ADC, a card with a good reflection surface, and a motor. The sensor has a numerical range of 0-255 (00-FF in hex) based on the distance between the sensor and the card.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My desired operation is: When I place my card near the sensor, the sensor will change its integer value and start the motor. And when the card is far from the sensor, the sensor value will increase and stop the motor. Here's my "half-working" code:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;void ADC_configuration (void)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;{&lt;BR /&gt;&amp;nbsp; ADC1SC1 = 0x20;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Interrupt disable. Continuous conversion mode and channel 0 active */&lt;BR /&gt;&amp;nbsp; ADC1SC2 = 0x20;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Compare enabled and triggers when input &amp;lt; compared value */&lt;BR /&gt;&amp;nbsp; ADCCFG = 0x30;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Input clock/2. Long Sample time configuration. 8-bit conversion */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp; ADC1CVL = 40;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* set compared value to 40 */&lt;BR /&gt;&amp;nbsp; ADC1SC1_COCO = 0;&lt;BR /&gt;}&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;void main(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; init_Motor();&amp;nbsp; /* Function that initializes the motor */&lt;BR /&gt;&amp;nbsp; ADC_configuration();&amp;nbsp; /* Function that initializes the ADC module */&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; EnableInterrupts; /* enable interrupts */&lt;BR /&gt;&amp;nbsp; ADC1SC1_AIEN = 1; /* Enable ADC interrupt */&lt;BR /&gt;&amp;nbsp; APCTL1_ADPC0 = 1; /* Select channel 0 for ADC input */&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; for(;; )&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __RESET_WATCHDOG();&lt;BR /&gt;&amp;nbsp; }&amp;nbsp;&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff;"&gt;interrupt 23 void ADC_input(void)&lt;BR /&gt;{&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; UINT8 temp;&lt;BR /&gt;&amp;nbsp; temp = ~ADC1RL;&lt;BR /&gt;&amp;nbsp; Motor_move();&amp;nbsp;&amp;nbsp;&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here's the problem: The program only works one time. Which means, if the card is close to the sensor when I start running the program, the motor will move. But if I remove the card from the sensor while the program is still running, the motor does not stop. And vice versa, where if the card is far from the sensor when I start running the program, the motor won't move. And if I place the card close to the sensor while the program is still running, the motor still won't move. Overall, it means that the sensor only reads once at the instantaneous point when the program starts running, and doesn't read at all after that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Help is appreciated. Thx&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by Cryptical on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-03-20&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;09:38 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="local-time"&gt;&amp;nbsp;Added p/n to subject.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by NLFSJ on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-03-20&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;09:21 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2009 16:36:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-help-on-using-ADC-interrupt-for-a-simple-operation/m-p/164892#M10335</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-03-20T16:36:30Z</dc:date>
    </item>
    <item>
      <title>Re: Need help on using ADC interrupt for a simple operation - MC9S08AW60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-help-on-using-ADC-interrupt-for-a-simple-operation/m-p/164893#M10336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've got it working already. The error was due to&amp;nbsp;some extra code in the for(;; ) loop, which I didn't include here. Thx&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2009 11:03:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Need-help-on-using-ADC-interrupt-for-a-simple-operation/m-p/164893#M10336</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-03-23T11:03:57Z</dc:date>
    </item>
  </channel>
</rss>