<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックQuestion about interrupts - MC9S08AW60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-about-interrupts-MC9S08AW60/m-p/164347#M10253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I'm using MC9S08AW60 MCU. I would like to ask if I'm able to use interrupts for pins that are not assigned to any "special" functions. For example, the pins PTE0 and PTE1 also function as the SCI1 Receive and&amp;nbsp;Transmit interface, therefore,&amp;nbsp;by checking&amp;nbsp;the datasheet, I'm able to use a particular&amp;nbsp;interrupt vector&amp;nbsp;number (17 in this case) to activate the SCI.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the pins PTF6 and PTF7 are not connected to any "special" functions like the SCI or TPM.&amp;nbsp;I've checked the pin connections&amp;nbsp;already.&amp;nbsp;Am I able to create an interrupt&amp;nbsp;by using these 2 pins? From the datasheet, it says vector numbers 26 through 31 are unused vector space that are available for user program. Not sure if I can assign PTF6 and PTF7 to them though&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Added p/n to subject.&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by NLFSJ on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-03-19&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;12:35 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2009 14:58:16 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2009-03-19T14:58:16Z</dc:date>
    <item>
      <title>Question about interrupts - MC9S08AW60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-about-interrupts-MC9S08AW60/m-p/164347#M10253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I'm using MC9S08AW60 MCU. I would like to ask if I'm able to use interrupts for pins that are not assigned to any "special" functions. For example, the pins PTE0 and PTE1 also function as the SCI1 Receive and&amp;nbsp;Transmit interface, therefore,&amp;nbsp;by checking&amp;nbsp;the datasheet, I'm able to use a particular&amp;nbsp;interrupt vector&amp;nbsp;number (17 in this case) to activate the SCI.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the pins PTF6 and PTF7 are not connected to any "special" functions like the SCI or TPM.&amp;nbsp;I've checked the pin connections&amp;nbsp;already.&amp;nbsp;Am I able to create an interrupt&amp;nbsp;by using these 2 pins? From the datasheet, it says vector numbers 26 through 31 are unused vector space that are available for user program. Not sure if I can assign PTF6 and PTF7 to them though&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Added p/n to subject.&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by NLFSJ on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-03-19&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;12:35 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2009 14:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-about-interrupts-MC9S08AW60/m-p/164347#M10253</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-03-19T14:58:16Z</dc:date>
    </item>
    <item>
      <title>Re: Question about interrupts</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-about-interrupts-MC9S08AW60/m-p/164348#M10254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;you can not assign interrupt vectors. This is done in Hardware.&amp;nbsp; If you need interrupts on input pins try to use KBI ports or use the IRQ Pin and check the port pins in your IRQ isr. Maybe some external extra logic is needed for that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eckhard&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2009 22:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-about-interrupts-MC9S08AW60/m-p/164348#M10254</guid>
      <dc:creator>eckhard</dc:creator>
      <dc:date>2009-03-19T22:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: Question about interrupts</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-about-interrupts-MC9S08AW60/m-p/164349#M10255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Ic. Thx for the reply &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2009 15:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Question-about-interrupts-MC9S08AW60/m-p/164349#M10255</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-03-20T15:49:29Z</dc:date>
    </item>
  </channel>
</rss>