<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: How to increase size of Tx and Rx Buffer in SMAC?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-increase-size-of-Tx-and-Rx-Buffer-in-SMAC/m-p/164255#M10222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Mou,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Yes,&amp;nbsp; a good question.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It has been a little while since I used the SMAC, but if I remember correctly, the SMAC puts the transceiver into packet mode. The maximum payload for the radio frame is 125 bytes. See the datasheet for the device, chapter 4.1.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It may be possible for you to increase the size of the transmitted and received packets from the MCU perspective, but these are needing to be fragmented before they are sent, or once they have been received. For that reason, I think that it is going to need a quite some thought for you to achieve what you want. The SMAC is going to stay the same, and you'll have to introduce your fragmentation management at the application layer.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Good lck,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Mark&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jun 2008 00:02:55 GMT</pubDate>
    <dc:creator>UK_CF_FAE</dc:creator>
    <dc:date>2008-06-18T00:02:55Z</dc:date>
    <item>
      <title>How to increase size of Tx and Rx Buffer in SMAC?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-increase-size-of-Tx-and-Rx-Buffer-in-SMAC/m-p/164254#M10221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone help me out regarding the Transmit and Receive Buffer size in SMAC? By default, SMAC supports TX and RX buffer size of 128. The structures for RX and TX packets, as defined in SMAC, are given below:-&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN style="color: #CC3333;"&gt;/*! defines the variable to be received by the SMAC */&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;typedef struct {&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&amp;nbsp;&amp;nbsp; UINT8 u8MaxDataLength; //!&amp;lt; maximum packet size to accept If greater packet is dropped&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;UINT8 u8DataLength;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; //!&amp;lt; length in bytes of the received packet&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;UINT8 *pu8Data;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; //!&amp;lt; where the application would like to have the received data copied into&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&amp;nbsp;&amp;nbsp; UINT8 u8Status;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; //!&amp;lt; determine if the data indication is due to a received packet or a timeout.&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;} tRxPacket;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;/*! variable to be transmitted by the SMAC.*/&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;typedef struct {&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; UINT8 u8DataLength; //!&amp;lt; number of bytes to transmit&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;UINT8 *pu8Data;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;//!&amp;lt; pointer to the data buffer to transmit&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #CC3333;"&gt;} tTxPacket;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have changed the datatypes of u8MaxDataLength and u8DataLength of tsRxPacket and u8DataLength of tsTxPacket to UINT16, so that it can accomodate more than 128 buffer elements. And, u8MaxDataLength has been initialized to value greater than 128. But, it is not working.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So, can anyone please suggest a way to transmit a packet containing more than 128 elements and can receive a packet of more than 128 elements?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mou&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jun 2008 18:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-increase-size-of-Tx-and-Rx-Buffer-in-SMAC/m-p/164254#M10221</guid>
      <dc:creator>mou</dc:creator>
      <dc:date>2008-06-13T18:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: How to increase size of Tx and Rx Buffer in SMAC?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-increase-size-of-Tx-and-Rx-Buffer-in-SMAC/m-p/164255#M10222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Mou,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Yes,&amp;nbsp; a good question.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It has been a little while since I used the SMAC, but if I remember correctly, the SMAC puts the transceiver into packet mode. The maximum payload for the radio frame is 125 bytes. See the datasheet for the device, chapter 4.1.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It may be possible for you to increase the size of the transmitted and received packets from the MCU perspective, but these are needing to be fragmented before they are sent, or once they have been received. For that reason, I think that it is going to need a quite some thought for you to achieve what you want. The SMAC is going to stay the same, and you'll have to introduce your fragmentation management at the application layer.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Good lck,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Mark&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jun 2008 00:02:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-increase-size-of-Tx-and-Rx-Buffer-in-SMAC/m-p/164255#M10222</guid>
      <dc:creator>UK_CF_FAE</dc:creator>
      <dc:date>2008-06-18T00:02:55Z</dc:date>
    </item>
  </channel>
</rss>