<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 mc9s08sh8 timer channels</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08sh8-timer-channels/m-p/164003#M10179</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am thinking of using the mc9s08sh8 model for my project since this microcontroller can work with 5V and has a DIP package. The number of I/O ports is very critical for me and in the datasheet it seems there are more than 2 TPM channels for each 16-bit timer module. I only need two channels for PWM signals and I couldn't figure it out which channels are for PWM. 7th and 11th pins are labeled as TPM1CH1 and 12th and 20th pins are labeled as TPM1CH0. Can anyone explain to me how these timer channels are configured?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 27 Dec 2009 23:15:54 GMT</pubDate>
    <dc:creator>hkaraoguz</dc:creator>
    <dc:date>2009-12-27T23:15:54Z</dc:date>
    <item>
      <title>mc9s08sh8 timer channels</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08sh8-timer-channels/m-p/164003#M10179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am thinking of using the mc9s08sh8 model for my project since this microcontroller can work with 5V and has a DIP package. The number of I/O ports is very critical for me and in the datasheet it seems there are more than 2 TPM channels for each 16-bit timer module. I only need two channels for PWM signals and I couldn't figure it out which channels are for PWM. 7th and 11th pins are labeled as TPM1CH1 and 12th and 20th pins are labeled as TPM1CH0. Can anyone explain to me how these timer channels are configured?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 Dec 2009 23:15:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08sh8-timer-channels/m-p/164003#M10179</guid>
      <dc:creator>hkaraoguz</dc:creator>
      <dc:date>2009-12-27T23:15:54Z</dc:date>
    </item>
    <item>
      <title>Re: mc9s08sh8 timer channels</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08sh8-timer-channels/m-p/164004#M10180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Have a peek at page 70 of the datasheet (System Options Register). It explains how you can choose which pins are timer I/O.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2009 05:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08sh8-timer-channels/m-p/164004#M10180</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-12-28T05:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: mc9s08sh8 timer channels</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08sh8-timer-channels/m-p/164005#M10181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thank you very much! Now, I have figured it out.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2009 03:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc9s08sh8-timer-channels/m-p/164005#M10181</guid>
      <dc:creator>hkaraoguz</dc:creator>
      <dc:date>2009-12-29T03:47:29Z</dc:date>
    </item>
  </channel>
</rss>